<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Can JTAG on NXP ARM MCUs be used for programming?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JTAG-on-NXP-ARM-MCUs-be-used-for-programming/m-p/1045404#M23093</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm evaluating the LPC11U6x family for a low-volume hobbyist project, but will automate PCBA production. A common approach is to use JTAG to verify the PCBA and upload code. JTAG is briefly described in the family datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, there's no mention of the ability to use JTAG to upload code. If this is not possible, can code be uploaded as a final production step via an external hardware interface rather than using the internal bootloader?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Aug 2020 04:21:14 GMT</pubDate>
    <dc:creator>phirung</dc:creator>
    <dc:date>2020-08-19T04:21:14Z</dc:date>
    <item>
      <title>Can JTAG on NXP ARM MCUs be used for programming?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JTAG-on-NXP-ARM-MCUs-be-used-for-programming/m-p/1045404#M23093</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm evaluating the LPC11U6x family for a low-volume hobbyist project, but will automate PCBA production. A common approach is to use JTAG to verify the PCBA and upload code. JTAG is briefly described in the family datasheet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, there's no mention of the ability to use JTAG to upload code. If this is not possible, can code be uploaded as a final production step via an external hardware interface rather than using the internal bootloader?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Aug 2020 04:21:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JTAG-on-NXP-ARM-MCUs-be-used-for-programming/m-p/1045404#M23093</guid>
      <dc:creator>phirung</dc:creator>
      <dc:date>2020-08-19T04:21:14Z</dc:date>
    </item>
    <item>
      <title>Re: Can JTAG on NXP ARM MCUs be used for programming?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JTAG-on-NXP-ARM-MCUs-be-used-for-programming/m-p/1045405#M23094</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Phirun Ng,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may use JTAG to upload the code to your device. You may find more details on how to connect using JTAG on the following Community Document.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/388998"&gt;https://community.nxp.com/thread/388998&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope that this helps!&lt;BR /&gt; Regards,&lt;/P&gt;&lt;P&gt;Gustavo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 15:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JTAG-on-NXP-ARM-MCUs-be-used-for-programming/m-p/1045405#M23094</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2020-08-20T15:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: Can JTAG on NXP ARM MCUs be used for programming?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JTAG-on-NXP-ARM-MCUs-be-used-for-programming/m-p/1045406#M23095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the advice and the link. Am still working through initial docn and finding my way around the site. All looking very promising.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Aug 2020 22:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-JTAG-on-NXP-ARM-MCUs-be-used-for-programming/m-p/1045406#M23095</guid>
      <dc:creator>phirung</dc:creator>
      <dc:date>2020-08-20T22:44:55Z</dc:date>
    </item>
  </channel>
</rss>