<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic AN3927 problem device cannot start with JM60 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN3927-problem-device-cannot-start-with-JM60/m-p/1040897#M23087</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i'm trying to use USB MSD bootloader with JM60 but when i connect the microcontroller to the HOST there is a message "device cannot start(code 10)" . Anyone had the same problem? How can i solve it?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm using Code warrior 6.3, AN3927 code reference and windows 10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 May 2020 16:31:47 GMT</pubDate>
    <dc:creator>eduardo1</dc:creator>
    <dc:date>2020-05-18T16:31:47Z</dc:date>
    <item>
      <title>AN3927 problem device cannot start with JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN3927-problem-device-cannot-start-with-JM60/m-p/1040897#M23087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, i'm trying to use USB MSD bootloader with JM60 but when i connect the microcontroller to the HOST there is a message "device cannot start(code 10)" . Anyone had the same problem? How can i solve it?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm using Code warrior 6.3, AN3927 code reference and windows 10.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 May 2020 16:31:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN3927-problem-device-cannot-start-with-JM60/m-p/1040897#M23087</guid>
      <dc:creator>eduardo1</dc:creator>
      <dc:date>2020-05-18T16:31:47Z</dc:date>
    </item>
    <item>
      <title>Re: AN3927 problem device cannot start with JM60</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN3927-problem-device-cannot-start-with-JM60/m-p/1040898#M23088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;The AN3927 is old, and there is not a new version for it, you can check the recommendation on the following thread&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/318424"&gt;https://community.nxp.com/thread/318424&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also codewarrior 6.3 is not recommended to run on windows 10, maybe you also have some problem with the windows driver&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 May 2020 15:15:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN3927-problem-device-cannot-start-with-JM60/m-p/1040898#M23088</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-05-20T15:15:08Z</dc:date>
    </item>
  </channel>
</rss>