<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 I want to find a car-grade chip with arctan computing function</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/I-want-to-find-a-car-grade-chip-with-arctan-computing-function/m-p/1023268#M23070</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The input signals are sin and cos signals. I want to use arctan calculation to convert them into angle data. I need to find a chip with arctan operation function? And I need to know how long does the arctan operation take?&lt;/P&gt;&lt;P&gt;1、I would like to ask if you have a chip with a CORDIC module？&lt;/P&gt;&lt;P&gt;2、Is there a chip that can calculate the arctan function? If so, how long does it take to calculate the arctan function once?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Feb 2020 05:36:05 GMT</pubDate>
    <dc:creator>ixhsun</dc:creator>
    <dc:date>2020-02-13T05:36:05Z</dc:date>
    <item>
      <title>I want to find a car-grade chip with arctan computing function</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/I-want-to-find-a-car-grade-chip-with-arctan-computing-function/m-p/1023268#M23070</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The input signals are sin and cos signals. I want to use arctan calculation to convert them into angle data. I need to find a chip with arctan operation function? And I need to know how long does the arctan operation take?&lt;/P&gt;&lt;P&gt;1、I would like to ask if you have a chip with a CORDIC module？&lt;/P&gt;&lt;P&gt;2、Is there a chip that can calculate the arctan function? If so, how long does it take to calculate the arctan function once?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Feb 2020 05:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/I-want-to-find-a-car-grade-chip-with-arctan-computing-function/m-p/1023268#M23070</guid>
      <dc:creator>ixhsun</dc:creator>
      <dc:date>2020-02-13T05:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: I want to find a car-grade chip with arctan computing function</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/I-want-to-find-a-car-grade-chip-with-arctan-computing-function/m-p/1023269#M23071</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do you want to use an 8 bit device for that?&lt;/P&gt;&lt;P&gt;please check the&amp;nbsp;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-architectures/8-bit-s08-mcus/8-bit-cost-effective-with-can-d-mcus:S08D"&gt;S08D family&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But maybe 32 bit devices is a better option&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Feb 2020 16:53:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/I-want-to-find-a-car-grade-chip-with-arctan-computing-function/m-p/1023269#M23071</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-02-14T16:53:00Z</dc:date>
    </item>
  </channel>
</rss>