<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックA question regarding MC9S08JM32 usb module power</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/A-question-regarding-MC9S08JM32-usb-module-power/m-p/995773#M23012</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm making a testing board using the MC9S08JM32 for USB applications but I'm not sure i understand the power situation, according to the datasheet the USB-B connector should be routed like so:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98705i26795E693D2B5CC0/image-size/large?v=v2&amp;amp;px=999" title="dgsdgasasdg.png" alt="dgsdgasasdg.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I've connected it like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99190iD5C7D0EEEED109FB/image-size/large?v=v2&amp;amp;px=999" title="gaewgdsg.png" alt="gaewgdsg.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In this design the VCC bar is either 3.3V or 5V depending on what source i connect to the board's power terminals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P4 is a 3-pin strip intended to use a jumper between pins 1&amp;amp;2 or 2&amp;amp;3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Vusb bar is connected to the MCU's VUSB33 pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is an error right?&lt;/P&gt;&lt;P&gt;I'm not sure I understand what Vbus or what is supposed to connect to, does it come from the Host(PC)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 20 Mar 2020 13:05:13 GMT</pubDate>
    <dc:creator>donperotti2</dc:creator>
    <dc:date>2020-03-20T13:05:13Z</dc:date>
    <item>
      <title>A question regarding MC9S08JM32 usb module power</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/A-question-regarding-MC9S08JM32-usb-module-power/m-p/995773#M23012</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I'm making a testing board using the MC9S08JM32 for USB applications but I'm not sure i understand the power situation, according to the datasheet the USB-B connector should be routed like so:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98705i26795E693D2B5CC0/image-size/large?v=v2&amp;amp;px=999" title="dgsdgasasdg.png" alt="dgsdgasasdg.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However I've connected it like this:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/99190iD5C7D0EEEED109FB/image-size/large?v=v2&amp;amp;px=999" title="gaewgdsg.png" alt="gaewgdsg.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In this design the VCC bar is either 3.3V or 5V depending on what source i connect to the board's power terminals.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P4 is a 3-pin strip intended to use a jumper between pins 1&amp;amp;2 or 2&amp;amp;3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Vusb bar is connected to the MCU's VUSB33 pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is an error right?&lt;/P&gt;&lt;P&gt;I'm not sure I understand what Vbus or what is supposed to connect to, does it come from the Host(PC)?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Mar 2020 13:05:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/A-question-regarding-MC9S08JM32-usb-module-power/m-p/995773#M23012</guid>
      <dc:creator>donperotti2</dc:creator>
      <dc:date>2020-03-20T13:05:13Z</dc:date>
    </item>
    <item>
      <title>Re: A question regarding MC9S08JM32 usb module power</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/A-question-regarding-MC9S08JM32-usb-module-power/m-p/995774#M23013</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PLease check&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103786iD220421A4B8141F2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Internally the USBDP is tied to VUSB33 through a pull up&lt;/P&gt;&lt;P&gt;I hope this will help you&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103831i32396918885500C3/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 17:54:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/A-question-regarding-MC9S08JM32-usb-module-power/m-p/995774#M23013</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2020-03-23T17:54:56Z</dc:date>
    </item>
  </channel>
</rss>