<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe:  MC908QY4 Replacement</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961275#M22995</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK. Tony! Nice to see a quick answer to my request. In fact I have used the FL16 for new designs, as it is a 32 SDIP package. However this FL16 is 8 bit PWM/ADC, I want to re make my question in the fact related to the features of the Microcontroller, currently the QY4 is already death for DIP package, however it has been a good friend during all this time of using it. But my main point is if there is a microcontroller with 10 bits ADC/PWM capability in DIP package.? at least not a pin to pin rplacement.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Oct 2019 22:05:53 GMT</pubDate>
    <dc:creator>miguelangelferr</dc:creator>
    <dc:date>2019-10-09T22:05:53Z</dc:date>
    <item>
      <title>MC908QY4 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961273#M22993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi My name is Miguel Angel Ferreira. I have been working by more than 5 years with the MC908QY4 8 Bits microcontroller. Now I want to update it to a more robust more faster but with the same DIP package microcotroller. I think that with 10 bits ADC and 10 bits PWM resolution I can greatly improve my current applications. So any suggestion??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 13:00:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961273#M22993</guid>
      <dc:creator>miguelangelferr</dc:creator>
      <dc:date>2019-10-09T13:00:51Z</dc:date>
    </item>
    <item>
      <title>Re:  MC908QY4 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961274#M22994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't think you will find a pin-to-pin replacement and HC08 does not seem to have much life left.&amp;nbsp; Maybe switch to 9S08.&lt;/P&gt;&lt;P&gt;The closest I can think (to give you more power and a DIP package) is the 9S08FL16.&amp;nbsp; But a board redesign, or at least an MCU replacement board, will be required.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 21:43:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961274#M22994</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2019-10-09T21:43:22Z</dc:date>
    </item>
    <item>
      <title>Re:  MC908QY4 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961275#M22995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK. Tony! Nice to see a quick answer to my request. In fact I have used the FL16 for new designs, as it is a 32 SDIP package. However this FL16 is 8 bit PWM/ADC, I want to re make my question in the fact related to the features of the Microcontroller, currently the QY4 is already death for DIP package, however it has been a good friend during all this time of using it. But my main point is if there is a microcontroller with 10 bits ADC/PWM capability in DIP package.? at least not a pin to pin rplacement.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 22:05:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961275#M22995</guid>
      <dc:creator>miguelangelferr</dc:creator>
      <dc:date>2019-10-09T22:05:53Z</dc:date>
    </item>
    <item>
      <title>Re:  MC908QY4 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961276#M22996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please check the s08qg family&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/products/processors-and-microcontrollers/additional-architectures/8-bit-s08-mcus/8-bit-small-package-qg-mcus:S08QG" title="https://www.nxp.com/products/processors-and-microcontrollers/additional-architectures/8-bit-s08-mcus/8-bit-small-package-qg-mcus:S08QG"&gt;8-bit Small Package QG MCUs | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is available on DIP8 and DIP16&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this will help you.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2019 19:30:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961276#M22996</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2019-10-10T19:30:57Z</dc:date>
    </item>
    <item>
      <title>Re:  MC908QY4 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961277#M22997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks!! many thanks! this is the answer I was looking for with my research! it fits my problem 100%. I can go further in my proyect now!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Oct 2019 20:49:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961277#M22997</guid>
      <dc:creator>miguelangelferr</dc:creator>
      <dc:date>2019-10-10T20:49:41Z</dc:date>
    </item>
    <item>
      <title>Re:  MC908QY4 Replacement</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961278#M22998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;A last buy date (May 2020) was just announced for 16-pin DIP QG4 / QG8.&amp;nbsp; Only the QG4 8-pin DIP survived (for now).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Dec 2019 12:09:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC908QY4-Replacement/m-p/961278#M22998</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2019-12-04T12:09:56Z</dc:date>
    </item>
  </channel>
</rss>