<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックTJA10152IT/5 no signal on RXD pin</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA10152IT-5-no-signal-on-RXD-pin/m-p/961076#M22991</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have TJA1052IT/5 used on the board to connect a radar sensor, there is a signal detected on CANH and CANL, but no signal on CANRXD pin. Is there something wrong or missed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Jun 2019 02:22:25 GMT</pubDate>
    <dc:creator>yangwenyou</dc:creator>
    <dc:date>2019-06-24T02:22:25Z</dc:date>
    <item>
      <title>TJA10152IT/5 no signal on RXD pin</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA10152IT-5-no-signal-on-RXD-pin/m-p/961076#M22991</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have TJA1052IT/5 used on the board to connect a radar sensor, there is a signal detected on CANH and CANL, but no signal on CANRXD pin. Is there something wrong or missed?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Jun 2019 02:22:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA10152IT-5-no-signal-on-RXD-pin/m-p/961076#M22991</guid>
      <dc:creator>yangwenyou</dc:creator>
      <dc:date>2019-06-24T02:22:25Z</dc:date>
    </item>
    <item>
      <title>Re: TJA10152IT/5 no signal on RXD pin</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA10152IT-5-no-signal-on-RXD-pin/m-p/961077#M22992</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Make sure that the TJA1052IT is set to normal mode.&lt;/P&gt;&lt;P&gt;The Normal Mode is entered setting pin STB to LOW. In Normal Mode Pin RXD reflects the normal CAN Receiver.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2019 15:04:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA10152IT-5-no-signal-on-RXD-pin/m-p/961077#M22992</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-06-26T15:04:18Z</dc:date>
    </item>
  </channel>
</rss>