<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ERROR L1907: Fixup overflow in  in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ERROR-L1907-Fixup-overflow-in/m-p/914527#M22911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm porting one project from MC09S08G16&amp;nbsp; to MX9S08DZ60. I've found multiple problems that has been fixed and now I'm stuck with this kind of message "&lt;EM&gt;ERROR L1907: Fixup overflow in Sys_Uart_Send_Byte, to VSys_Uart_Tx type 1, at offset 0x3".&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not particular from this module, because If I comment this code appear another "&lt;EM&gt;ERROR L1907: Fixup overflow in&amp;nbsp;..."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does anyone that any idea that could cause this problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Aug 2019 13:01:36 GMT</pubDate>
    <dc:creator>hardware</dc:creator>
    <dc:date>2019-08-12T13:01:36Z</dc:date>
    <item>
      <title>ERROR L1907: Fixup overflow in</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ERROR-L1907-Fixup-overflow-in/m-p/914527#M22911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm porting one project from MC09S08G16&amp;nbsp; to MX9S08DZ60. I've found multiple problems that has been fixed and now I'm stuck with this kind of message "&lt;EM&gt;ERROR L1907: Fixup overflow in Sys_Uart_Send_Byte, to VSys_Uart_Tx type 1, at offset 0x3".&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's not particular from this module, because If I comment this code appear another "&lt;EM&gt;ERROR L1907: Fixup overflow in&amp;nbsp;..."&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Does anyone that any idea that could cause this problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Best Regards&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 13:01:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ERROR-L1907-Fixup-overflow-in/m-p/914527#M22911</guid>
      <dc:creator>hardware</dc:creator>
      <dc:date>2019-08-12T13:01:36Z</dc:date>
    </item>
    <item>
      <title>Re: ERROR L1907: Fixup overflow in</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ERROR-L1907-Fixup-overflow-in/m-p/914528#M22912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problems seems to be located at ISR routine, when I use global variable&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void uart1_tx_ISR(void)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;STRONG&gt;&amp;nbsp;&amp;nbsp;VSys_Uart_Tx_Complete=1;&lt;/STRONG&gt;&lt;BR /&gt; &lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;SCI1C2=V_SCIC2; &lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then appears error &lt;EM&gt;"ERROR L1907: Fixup overflow in uart1_tx_ISR, to VSys_Uart_Tx_Complete type 1, at offset 0x5"&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2019 09:44:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ERROR-L1907-Fixup-overflow-in/m-p/914528#M22912</guid>
      <dc:creator>hardware</dc:creator>
      <dc:date>2019-08-13T09:44:36Z</dc:date>
    </item>
  </channel>
</rss>