<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: on delay</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/on-delay/m-p/892396#M22845</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not good in ASM code and this is very old, but I am not sure that the code is complete.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 17 May 2019 17:56:07 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2019-05-17T17:56:07Z</dc:date>
    <item>
      <title>on delay</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/on-delay/m-p/892395#M22844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Off Delay type changed to on delay type.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Dear sir,&lt;/P&gt;&lt;P&gt;Attach relay control part source.&lt;/P&gt;&lt;P&gt;The current relay time delay is an&amp;nbsp;OFF&amp;nbsp;DELAY type. We want to change this to&amp;nbsp;ON&amp;nbsp;DELAY type.&lt;/P&gt;&lt;P&gt;That is, it is necessary to change the output to "on" after a certain time after the input is turned on. There are no conditions (people, tools, etc.) to do this, and we ask for support(help).&lt;/P&gt;&lt;P&gt;It is really urgent.&lt;/P&gt;&lt;P&gt;In addition, the entire program source is attached. Please refer.&lt;/P&gt;&lt;P&gt;Device is MC68HC705.&lt;/P&gt;&lt;P&gt;This&amp;nbsp;is a program made in motorola assembly language.&lt;/P&gt;&lt;P&gt;I will be waiting for your quick reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 19:32:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/on-delay/m-p/892395#M22844</guid>
      <dc:creator>jakjeon2</dc:creator>
      <dc:date>2019-05-13T19:32:01Z</dc:date>
    </item>
    <item>
      <title>Re: on delay</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/on-delay/m-p/892396#M22845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not good in ASM code and this is very old, but I am not sure that the code is complete.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 May 2019 17:56:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/on-delay/m-p/892396#M22845</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2019-05-17T17:56:07Z</dc:date>
    </item>
    <item>
      <title>Re: on delay</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/on-delay/m-p/892397#M22846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is certainly not a complete program.&amp;nbsp; It lacks a whole bunch of symbol definitions, a reset vector, proper initialization, etc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 17 May 2019 21:33:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/on-delay/m-p/892397#M22846</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2019-05-17T21:33:44Z</dc:date>
    </item>
  </channel>
</rss>