<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 p89lpc92 kbi</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/p89lpc92-kbi/m-p/891771#M22833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The KBI does not function in a P89LPC921F but it functions in the P89LPC925F.&lt;/P&gt;&lt;P&gt;In the 921 the KBPATN always has a value of "0FFH" and the KBMASK always has a value of "00".&amp;nbsp; If I write the registers and read back the value, it is unchanged.&amp;nbsp; I assume that since the KBMASK is "00", that is why an interrupt never occurs.&amp;nbsp; Is anyone else aware of this problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 11 Apr 2019 01:36:33 GMT</pubDate>
    <dc:creator>rotsig</dc:creator>
    <dc:date>2019-04-11T01:36:33Z</dc:date>
    <item>
      <title>p89lpc92 kbi</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/p89lpc92-kbi/m-p/891771#M22833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The KBI does not function in a P89LPC921F but it functions in the P89LPC925F.&lt;/P&gt;&lt;P&gt;In the 921 the KBPATN always has a value of "0FFH" and the KBMASK always has a value of "00".&amp;nbsp; If I write the registers and read back the value, it is unchanged.&amp;nbsp; I assume that since the KBMASK is "00", that is why an interrupt never occurs.&amp;nbsp; Is anyone else aware of this problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Apr 2019 01:36:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/p89lpc92-kbi/m-p/891771#M22833</guid>
      <dc:creator>rotsig</dc:creator>
      <dc:date>2019-04-11T01:36:33Z</dc:date>
    </item>
  </channel>
</rss>