<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Use BDFR instead of Reset pin when programming MC9S08PA16 ?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Use-BDFR-instead-of-Reset-pin-when-programming-MC9S08PA16/m-p/885330#M22817</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excellent!&lt;/P&gt;&lt;P&gt;Thank you Vicente :-)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Apr 2019 12:25:19 GMT</pubDate>
    <dc:creator>JimDandy</dc:creator>
    <dc:date>2019-04-10T12:25:19Z</dc:date>
    <item>
      <title>Use BDFR instead of Reset pin when programming MC9S08PA16 ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Use-BDFR-instead-of-Reset-pin-when-programming-MC9S08PA16/m-p/885328#M22815</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have used 705 and 908 micros many times in the past, and just now starting my first board using both in-system-programming and S08 micros. It's an update of a 908 board and everything is written in assembly. I've just discovered that PORT A5 is also IRQ and RESET. I've used the BIH and BIL instruction frequently in the code and I'd rather not change it if I don't have to. Sharing pins looks messy. So... does the reset pin *have* to be connected to the BDM connector and the programmer or will the programmer set the BDFR bit and do a reset like that. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Apr 2019 10:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Use-BDFR-instead-of-Reset-pin-when-programming-MC9S08PA16/m-p/885328#M22815</guid>
      <dc:creator>JimDandy</dc:creator>
      <dc:date>2019-04-08T10:02:10Z</dc:date>
    </item>
    <item>
      <title>Re: Use BDFR instead of Reset pin when programming MC9S08PA16 ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Use-BDFR-instead-of-Reset-pin-when-programming-MC9S08PA16/m-p/885329#M22816</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Yes, the programmer can do the BDRF without the reset pin, just you need to do a power cycle (turn off and turn on the device).&lt;/P&gt;&lt;P&gt;I hope this will help you.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Apr 2019 21:18:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Use-BDFR-instead-of-Reset-pin-when-programming-MC9S08PA16/m-p/885329#M22816</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2019-04-09T21:18:27Z</dc:date>
    </item>
    <item>
      <title>Re: Use BDFR instead of Reset pin when programming MC9S08PA16 ?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Use-BDFR-instead-of-Reset-pin-when-programming-MC9S08PA16/m-p/885330#M22817</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Excellent!&lt;/P&gt;&lt;P&gt;Thank you Vicente :-)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2019 12:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Use-BDFR-instead-of-Reset-pin-when-programming-MC9S08PA16/m-p/885330#M22817</guid>
      <dc:creator>JimDandy</dc:creator>
      <dc:date>2019-04-10T12:25:19Z</dc:date>
    </item>
  </channel>
</rss>