<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: MOSI Low level</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MOSI-Low-level/m-p/860138#M22735</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same problem when I chose to use the SPI for driving the sk68xx RGB LED, and the quick answer is you can't change this behavior of the SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My solution was to invert the line and send inverted data.&amp;nbsp; It worked perfectly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 02 Mar 2019 23:08:43 GMT</pubDate>
    <dc:creator>tonyp</dc:creator>
    <dc:date>2019-03-02T23:08:43Z</dc:date>
    <item>
      <title>MOSI Low level</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MOSI-Low-level/m-p/860137#M22734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have S08AC32, I use the SPI uart, there is a possibility to have the MOSI signal at low level at the end of transmission ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stefano De Blasiis&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Mar 2019 10:07:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MOSI-Low-level/m-p/860137#M22734</guid>
      <dc:creator>IlConte</dc:creator>
      <dc:date>2019-03-01T10:07:59Z</dc:date>
    </item>
    <item>
      <title>Re: MOSI Low level</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MOSI-Low-level/m-p/860138#M22735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had the same problem when I chose to use the SPI for driving the sk68xx RGB LED, and the quick answer is you can't change this behavior of the SPI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My solution was to invert the line and send inverted data.&amp;nbsp; It worked perfectly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Mar 2019 23:08:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MOSI-Low-level/m-p/860138#M22735</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2019-03-02T23:08:43Z</dc:date>
    </item>
  </channel>
</rss>