<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FXTH871 PWU Flag Bits Unresponsive in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH871-PWU-Flag-Bits-Unresponsive/m-p/843451#M22684</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running in to a problem with the FXTH871, in particular with the PWU Flag Bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 2 flag bits that I can see that on the datasheet say will be set whenever a Periodic Wake Up is what removes the MCU from SLEEP modes.&amp;nbsp; These 2 bits are: PWUCS0_WUF &amp;amp; SIMSES_PWUF.&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;*From the datasheet:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PWUCS0_WUF: Wakeup Interrupt Flag — The WUF bit indicates when a wakeup interrupt has been generated by the PWU. This bit is cleared by writing a one to the WUFAK bit. Writing a zero to this bit has no effect. Reset clears this bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIMSES_PWUF:&amp;nbsp;PWU Flag — This bit indicates that the PWU module caused the last exit from STOP mode.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Neither of these bits seems to be set when I use PWU to wake up the MCU from SLEEP modes.&amp;nbsp; I am certain that the PWU is responsible for the wake up as well because I can adjust the time on the PWU, and it correctly wakes up at whatever time I set it to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached the very simple code that I am running right now to this post.&amp;nbsp; I am hoping that somebody can answer to me&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Jul 2018 18:09:37 GMT</pubDate>
    <dc:creator>csaunders9526</dc:creator>
    <dc:date>2018-07-03T18:09:37Z</dc:date>
    <item>
      <title>FXTH871 PWU Flag Bits Unresponsive</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH871-PWU-Flag-Bits-Unresponsive/m-p/843451#M22684</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running in to a problem with the FXTH871, in particular with the PWU Flag Bits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are 2 flag bits that I can see that on the datasheet say will be set whenever a Periodic Wake Up is what removes the MCU from SLEEP modes.&amp;nbsp; These 2 bits are: PWUCS0_WUF &amp;amp; SIMSES_PWUF.&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;*From the datasheet:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PWUCS0_WUF: Wakeup Interrupt Flag — The WUF bit indicates when a wakeup interrupt has been generated by the PWU. This bit is cleared by writing a one to the WUFAK bit. Writing a zero to this bit has no effect. Reset clears this bit.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SIMSES_PWUF:&amp;nbsp;PWU Flag — This bit indicates that the PWU module caused the last exit from STOP mode.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;----------------------------------------------------------------------------------------------------------------------------------------&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Neither of these bits seems to be set when I use PWU to wake up the MCU from SLEEP modes.&amp;nbsp; I am certain that the PWU is responsible for the wake up as well because I can adjust the time on the PWU, and it correctly wakes up at whatever time I set it to.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached the very simple code that I am running right now to this post.&amp;nbsp; I am hoping that somebody can answer to me&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Jul 2018 18:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH871-PWU-Flag-Bits-Unresponsive/m-p/843451#M22684</guid>
      <dc:creator>csaunders9526</dc:creator>
      <dc:date>2018-07-03T18:09:37Z</dc:date>
    </item>
  </channel>
</rss>