<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic eeprom segment in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/eeprom-segment/m-p/834969#M22680</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a S08 PT60 processor with codewarrior 10.6.4&lt;/P&gt;&lt;P&gt;I need to inizilize the eeprom value.&lt;/P&gt;&lt;P&gt;I have try to use a array definition :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// default eeprom value&lt;BR /&gt;const uint8_t EEdefault&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [16] @0x3100 = {0x00, 0x05, 0x05, 0x14, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};&amp;nbsp; &amp;nbsp;&lt;BR /&gt;const uint8_t EEdefaultcpl&amp;nbsp; [16] @0x3110 = {0xFF, 0xFA, 0xFA, 0xEB, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};&amp;nbsp; &amp;nbsp;&lt;BR /&gt;const uint8_t EEdefault1&amp;nbsp;&amp;nbsp;&amp;nbsp; [16] @0x3120 = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};&amp;nbsp; &amp;nbsp;&lt;BR /&gt;const uint8_t EEdefault1cpl [16] @0x3130 = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But don't work ! Why ?&lt;/P&gt;&lt;P&gt;I need to add a segment definition ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Dec 2018 08:00:11 GMT</pubDate>
    <dc:creator>IlConte</dc:creator>
    <dc:date>2018-12-05T08:00:11Z</dc:date>
    <item>
      <title>eeprom segment</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/eeprom-segment/m-p/834969#M22680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a S08 PT60 processor with codewarrior 10.6.4&lt;/P&gt;&lt;P&gt;I need to inizilize the eeprom value.&lt;/P&gt;&lt;P&gt;I have try to use a array definition :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;// default eeprom value&lt;BR /&gt;const uint8_t EEdefault&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [16] @0x3100 = {0x00, 0x05, 0x05, 0x14, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00};&amp;nbsp; &amp;nbsp;&lt;BR /&gt;const uint8_t EEdefaultcpl&amp;nbsp; [16] @0x3110 = {0xFF, 0xFA, 0xFA, 0xEB, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};&amp;nbsp; &amp;nbsp;&lt;BR /&gt;const uint8_t EEdefault1&amp;nbsp;&amp;nbsp;&amp;nbsp; [16] @0x3120 = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};&amp;nbsp; &amp;nbsp;&lt;BR /&gt;const uint8_t EEdefault1cpl [16] @0x3130 = {0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF, 0xFF};&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But don't work ! Why ?&lt;/P&gt;&lt;P&gt;I need to add a segment definition ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Stefano&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Dec 2018 08:00:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/eeprom-segment/m-p/834969#M22680</guid>
      <dc:creator>IlConte</dc:creator>
      <dc:date>2018-12-05T08:00:11Z</dc:date>
    </item>
  </channel>
</rss>