<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic RAM in FXTH870000 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RAM-in-FXTH870000/m-p/831058#M22667</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, this is with reference to FXTH870000 series. Does the FLASH transfer executable code to the RAM first before execution.&lt;/P&gt;&lt;P&gt;Of the 512 bytes of RAM space available, how much RAM space would be free for me to store some additional data? Do I have to account for the space that the code from FLASH to RAM will take while bootloading ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Aug 2018 05:07:46 GMT</pubDate>
    <dc:creator>f20150335</dc:creator>
    <dc:date>2018-08-28T05:07:46Z</dc:date>
    <item>
      <title>RAM in FXTH870000</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RAM-in-FXTH870000/m-p/831058#M22667</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, this is with reference to FXTH870000 series. Does the FLASH transfer executable code to the RAM first before execution.&lt;/P&gt;&lt;P&gt;Of the 512 bytes of RAM space available, how much RAM space would be free for me to store some additional data? Do I have to account for the space that the code from FLASH to RAM will take while bootloading ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Aug 2018 05:07:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RAM-in-FXTH870000/m-p/831058#M22667</guid>
      <dc:creator>f20150335</dc:creator>
      <dc:date>2018-08-28T05:07:46Z</dc:date>
    </item>
  </channel>
</rss>