<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Can a JM60 be programmed directly from the USBDN and USBDP pins to a PC, without the need for an intermediate device (PEmicro, multilink, etc.)? in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-a-JM60-be-programmed-directly-from-the-USBDN-and-USBDP-pins/m-p/829133#M22663</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! I have a board of a device that I disarmed that brings a JM60. Investigating the board and the datasheet of the JM60, I saw that it brings a USB card connected to the pins USBDP, USBDN, VDD and VSS, also brings a 6-pin BKGD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is this, is it possible to connect it to a PC directly with a USB cable, which is detected, and load the program with the CodeWarrior? Is it possible to do this without the need of a JTAG or a programming device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, the functionality for which the board was manufactured is lost, but that is not the problem ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance, and know excuse my ignorance in the subject&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 23 Dec 2018 02:28:38 GMT</pubDate>
    <dc:creator>alan36alexis</dc:creator>
    <dc:date>2018-12-23T02:28:38Z</dc:date>
    <item>
      <title>Can a JM60 be programmed directly from the USBDN and USBDP pins to a PC, without the need for an intermediate device (PEmicro, multilink, etc.)?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-a-JM60-be-programmed-directly-from-the-USBDN-and-USBDP-pins/m-p/829133#M22663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello! I have a board of a device that I disarmed that brings a JM60. Investigating the board and the datasheet of the JM60, I saw that it brings a USB card connected to the pins USBDP, USBDN, VDD and VSS, also brings a 6-pin BKGD.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is this, is it possible to connect it to a PC directly with a USB cable, which is detected, and load the program with the CodeWarrior? Is it possible to do this without the need of a JTAG or a programming device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Obviously, the functionality for which the board was manufactured is lost, but that is not the problem ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance, and know excuse my ignorance in the subject&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Dec 2018 02:28:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-a-JM60-be-programmed-directly-from-the-USBDN-and-USBDP-pins/m-p/829133#M22663</guid>
      <dc:creator>alan36alexis</dc:creator>
      <dc:date>2018-12-23T02:28:38Z</dc:date>
    </item>
    <item>
      <title>Re: Can a JM60 be programmed directly from the USBDN and USBDP pins to a PC, without the need for an intermediate device (PEmicro, multilink, etc.)?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-a-JM60-be-programmed-directly-from-the-USBDN-and-USBDP-pins/m-p/829134#M22664</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;As I know this is not possible.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Jan 2019 17:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Can-a-JM60-be-programmed-directly-from-the-USBDN-and-USBDP-pins/m-p/829134#M22664</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2019-01-03T17:13:17Z</dc:date>
    </item>
  </channel>
</rss>