<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックI need to have MC9S08QD4 programed</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/I-need-to-have-MC9S08QD4-programed/m-p/818681#M22644</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a couple of MC9S08QD4 programed as specified in NXP document&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN3602.pdf" title="https://www.nxp.com/docs/en/application-note/AN3602.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3602.pdf&lt;/A&gt;&amp;nbsp; &amp;nbsp;I am working on an idle air control valve on my Corvair.&amp;nbsp; The Microsquirt using PWM in duty&amp;nbsp;percentages of 0-100 and I have a L298N to control the higher current stepper motors.&amp;nbsp; &amp;nbsp;Duty to steps should be 1 to 1 (max 100 steps) which if I ready correctly is how the programing instructions in AN3602 is set. The PWM was intended to drive a PWM idle solinoid with negative control and 12VDC (if that helps).&amp;nbsp; The L298N will provide the 5VDC I will need to power the MC0S08QD4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really dont want to spend all the cash on programing equipment and ardrino code may be at end of my capabilities.&amp;nbsp; The chip as spelled out in this document may be perfect for what I need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I dont want this for free of course.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ted&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Aug 2018 12:43:01 GMT</pubDate>
    <dc:creator>ted1</dc:creator>
    <dc:date>2018-08-23T12:43:01Z</dc:date>
    <item>
      <title>I need to have MC9S08QD4 programed</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/I-need-to-have-MC9S08QD4-programed/m-p/818681#M22644</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need a couple of MC9S08QD4 programed as specified in NXP document&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN3602.pdf" title="https://www.nxp.com/docs/en/application-note/AN3602.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN3602.pdf&lt;/A&gt;&amp;nbsp; &amp;nbsp;I am working on an idle air control valve on my Corvair.&amp;nbsp; The Microsquirt using PWM in duty&amp;nbsp;percentages of 0-100 and I have a L298N to control the higher current stepper motors.&amp;nbsp; &amp;nbsp;Duty to steps should be 1 to 1 (max 100 steps) which if I ready correctly is how the programing instructions in AN3602 is set. The PWM was intended to drive a PWM idle solinoid with negative control and 12VDC (if that helps).&amp;nbsp; The L298N will provide the 5VDC I will need to power the MC0S08QD4.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I really dont want to spend all the cash on programing equipment and ardrino code may be at end of my capabilities.&amp;nbsp; The chip as spelled out in this document may be perfect for what I need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I dont want this for free of course.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ted&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Aug 2018 12:43:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/I-need-to-have-MC9S08QD4-programed/m-p/818681#M22644</guid>
      <dc:creator>ted1</dc:creator>
      <dc:date>2018-08-23T12:43:01Z</dc:date>
    </item>
  </channel>
</rss>