<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Bootloader for P89LPC936</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-for-P89LPC936/m-p/801478#M22607</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;I have accidentally set the wrong secure bits (Block 0 Sec 1 and 2) on a P89LPC936. The only way I found to clear them was to erase the complete flash including the bootloader. Is there any possibility to clear them, without erasing the bootloader?&lt;/P&gt;&lt;P&gt;If not, I think it should be possible to reprogram the &lt;A href="https://community.nxp.com/t5/tag/bootloader/tg-p"&gt;#bootloader&lt;/A&gt; again. But I do not have the HEX-file for the bootloader. Is it possible to download it somewhere? Or is there a way to read it from a working second chip?&lt;/P&gt;&lt;P&gt;Any help is welcome. Thanx a lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Philip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Nov 2018 13:03:20 GMT</pubDate>
    <dc:creator>p_weigl</dc:creator>
    <dc:date>2018-11-05T13:03:20Z</dc:date>
    <item>
      <title>Bootloader for P89LPC936</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-for-P89LPC936/m-p/801478#M22607</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;I have accidentally set the wrong secure bits (Block 0 Sec 1 and 2) on a P89LPC936. The only way I found to clear them was to erase the complete flash including the bootloader. Is there any possibility to clear them, without erasing the bootloader?&lt;/P&gt;&lt;P&gt;If not, I think it should be possible to reprogram the &lt;A href="https://community.nxp.com/t5/tag/bootloader/tg-p"&gt;#bootloader&lt;/A&gt; again. But I do not have the HEX-file for the bootloader. Is it possible to download it somewhere? Or is there a way to read it from a working second chip?&lt;/P&gt;&lt;P&gt;Any help is welcome. Thanx a lot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Philip&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 13:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-for-P89LPC936/m-p/801478#M22607</guid>
      <dc:creator>p_weigl</dc:creator>
      <dc:date>2018-11-05T13:03:20Z</dc:date>
    </item>
  </channel>
</rss>