<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックCalling Firmware Functions in FXTH87xxDD</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Calling-Firmware-Functions-in-FXTH87xxDD/m-p/793537#M22597</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i cannot get the result in the register when I am multiplying two numbers using the following code -&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63065i9835525C52D7B499/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Am I completely incorrect in calling the function. How should it be done?&amp;nbsp; When i write TPMS_MULT_SIGN_INT16 I get an error message too. So what should I do to call this function?&lt;/P&gt;&lt;P&gt;I am only implementing this function for learning as later I would have to call the read_pressure type functions too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Aug 2018 06:31:19 GMT</pubDate>
    <dc:creator>f20150335</dc:creator>
    <dc:date>2018-08-16T06:31:19Z</dc:date>
    <item>
      <title>Calling Firmware Functions in FXTH87xxDD</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Calling-Firmware-Functions-in-FXTH87xxDD/m-p/793537#M22597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, i cannot get the result in the register when I am multiplying two numbers using the following code -&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/63065i9835525C52D7B499/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Am I completely incorrect in calling the function. How should it be done?&amp;nbsp; When i write TPMS_MULT_SIGN_INT16 I get an error message too. So what should I do to call this function?&lt;/P&gt;&lt;P&gt;I am only implementing this function for learning as later I would have to call the read_pressure type functions too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Aug 2018 06:31:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Calling-Firmware-Functions-in-FXTH87xxDD/m-p/793537#M22597</guid>
      <dc:creator>f20150335</dc:creator>
      <dc:date>2018-08-16T06:31:19Z</dc:date>
    </item>
  </channel>
</rss>