<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックFXTH87  - Giving strange values sometimes</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH87-Giving-strange-values-sometimes/m-p/783600#M22587</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using the FXTH87 TPMS for getting pressure readings through SPI on another device. I have disabled the RF module. But sometimes it gives very strange random values like Temperature as (-55), 110; voltage as 60 V etc and similar thing happens with the pressure readings as well.&lt;/P&gt;&lt;P&gt;What can be the causes behind these issues? Any suggestions are welcome. Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Oct 2018 03:20:54 GMT</pubDate>
    <dc:creator>f20150335</dc:creator>
    <dc:date>2018-10-31T03:20:54Z</dc:date>
    <item>
      <title>FXTH87  - Giving strange values sometimes</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH87-Giving-strange-values-sometimes/m-p/783600#M22587</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am using the FXTH87 TPMS for getting pressure readings through SPI on another device. I have disabled the RF module. But sometimes it gives very strange random values like Temperature as (-55), 110; voltage as 60 V etc and similar thing happens with the pressure readings as well.&lt;/P&gt;&lt;P&gt;What can be the causes behind these issues? Any suggestions are welcome. Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 03:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH87-Giving-strange-values-sometimes/m-p/783600#M22587</guid>
      <dc:creator>f20150335</dc:creator>
      <dc:date>2018-10-31T03:20:54Z</dc:date>
    </item>
  </channel>
</rss>