<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Freescale MCU s9s08dz60 secured</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-MCU-s9s08dz60-secured/m-p/761072#M22546</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你好:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;我看到你有一个相同的问题:&lt;A href="https://community.nxp.com/message/973357"&gt;https://community.nxp.com/message/973357&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;请尽量详细的提供片子的批次信息和MASKSET, 我们需要这些信息来评估产品的问题,谢谢!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jan 2018 08:49:42 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2018-01-15T08:49:42Z</dc:date>
    <item>
      <title>Freescale MCU s9s08dz60 secured</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-MCU-s9s08dz60-secured/m-p/761071#M22545</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ten mature pieces of pcb production,but the program is only a piece of could have gone under ,the rest were promt chip is secured,unsecured success is lower,but the application of chip with the previously entered into under this batch of can go in,then found that as long as you can in the program,has been entered .There have been no such problem before.It dosen,t like the boad problem,because someone can be download.thank you !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jan 2018 08:02:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-MCU-s9s08dz60-secured/m-p/761071#M22545</guid>
      <dc:creator>chunpingxu</dc:creator>
      <dc:date>2018-01-04T08:02:43Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale MCU s9s08dz60 secured</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-MCU-s9s08dz60-secured/m-p/761072#M22546</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;你好:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;我看到你有一个相同的问题:&lt;A href="https://community.nxp.com/message/973357"&gt;https://community.nxp.com/message/973357&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;请尽量详细的提供片子的批次信息和MASKSET, 我们需要这些信息来评估产品的问题,谢谢!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 08:49:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-MCU-s9s08dz60-secured/m-p/761072#M22546</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2018-01-15T08:49:42Z</dc:date>
    </item>
    <item>
      <title>Re: Freescale MCU s9s08dz60 secured</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-MCU-s9s08dz60-secured/m-p/1491120#M23546</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Dear NXP Semiconductors,&amp;nbsp; I'm a Freescale MCU user. I mainly use this chip s9s08dz60. After downloading the program, I can't read it after encryption. Many times, the original code is lost. I need to read the encrypted program, so I want to apply for a software with you, or the engineering software or backdoor software of this chip, In general, it is the software that can read the encrypted flash program of this chip. Thank you. If you can provide it, send it to my email,&amp;nbsp;&lt;/SPAN&gt;&lt;A href="mailto:361627335@qq.com" target="_blank" rel="noopener"&gt;361627335@qq.com&lt;/A&gt;&lt;SPAN&gt;&amp;nbsp;, thank you again.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 18 Jul 2022 15:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Freescale-MCU-s9s08dz60-secured/m-p/1491120#M23546</guid>
      <dc:creator>yongzhu</dc:creator>
      <dc:date>2022-07-18T15:06:20Z</dc:date>
    </item>
  </channel>
</rss>