<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TJA1043 Bus Off is not detecting (CANH or CANL is open) in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA1043-Bus-Off-is-not-detecting-CANH-or-CANL-is-open/m-p/746068#M22516</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I need a clarification related to Bus Off detection, dependency with CAN transceiver.&lt;/P&gt;&lt;P&gt;Transceiver : TJA1043&lt;/P&gt;&lt;P&gt;Controller: Renesas RH850&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During&amp;nbsp;my testing on the Bus Off detection,&amp;nbsp;I have observed that in the&lt;/P&gt;&lt;P&gt;following scenarios, Bus Off detection is not happening.&lt;/P&gt;&lt;P&gt;- CAN_H is connected and CAN_L is opened&lt;/P&gt;&lt;P&gt;- CAN_H is opened (not connected) and CAN_L is connected.&lt;/P&gt;&lt;P&gt;I would like to understand is there any limitation with the&amp;nbsp;TJA1043 in&lt;/P&gt;&lt;P&gt;detecting the above scenario ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tja1043‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Jan 2018 02:30:42 GMT</pubDate>
    <dc:creator>shanmugamsundar</dc:creator>
    <dc:date>2018-01-23T02:30:42Z</dc:date>
    <item>
      <title>TJA1043 Bus Off is not detecting (CANH or CANL is open)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA1043-Bus-Off-is-not-detecting-CANH-or-CANL-is-open/m-p/746068#M22516</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I need a clarification related to Bus Off detection, dependency with CAN transceiver.&lt;/P&gt;&lt;P&gt;Transceiver : TJA1043&lt;/P&gt;&lt;P&gt;Controller: Renesas RH850&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;During&amp;nbsp;my testing on the Bus Off detection,&amp;nbsp;I have observed that in the&lt;/P&gt;&lt;P&gt;following scenarios, Bus Off detection is not happening.&lt;/P&gt;&lt;P&gt;- CAN_H is connected and CAN_L is opened&lt;/P&gt;&lt;P&gt;- CAN_H is opened (not connected) and CAN_L is connected.&lt;/P&gt;&lt;P&gt;I would like to understand is there any limitation with the&amp;nbsp;TJA1043 in&lt;/P&gt;&lt;P&gt;detecting the above scenario ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tja1043‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Jan 2018 02:30:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA1043-Bus-Off-is-not-detecting-CANH-or-CANL-is-open/m-p/746068#M22516</guid>
      <dc:creator>shanmugamsundar</dc:creator>
      <dc:date>2018-01-23T02:30:42Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 Bus Off is not detecting</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA1043-Bus-Off-is-not-detecting-CANH-or-CANL-is-open/m-p/746069#M22517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;I have found a FMEA matrix table from the Application hints document for TJA1043.&lt;/P&gt;&lt;P&gt;In that it says that if CANH or CANL is open &lt;STRONG&gt;Transmission not possible. &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have confusion, if&amp;nbsp;controller tries to transmits the messages in this scenario,(i.e. CANH or CANL open), will it detect the transmit error or the No acknowledgement error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope there will be a no acknowledgement error. Because if CANH or CANL is open still Controller can able to read backs the information what it has sent successfully.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is it correct? can someone please clear my confusion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="FMEA_Matrix.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/20893i7FE0B1A9E6D16CD3/image-size/large?v=v2&amp;amp;px=999" role="button" title="FMEA_Matrix.png" alt="FMEA_Matrix.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Shan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 03:08:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA1043-Bus-Off-is-not-detecting-CANH-or-CANL-is-open/m-p/746069#M22517</guid>
      <dc:creator>shanmugamsundar</dc:creator>
      <dc:date>2018-01-24T03:08:01Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1043 Bus Off is not detecting</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA1043-Bus-Off-is-not-detecting-CANH-or-CANL-is-open/m-p/746070#M22518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;As per the clarification got from NXP, The CAN controller can able to read back its own sent messages even though the bus line is open.&lt;/P&gt;&lt;P&gt;Hence, there won't be a chance of transmit error count, only the receive error count will get increased due to no acknowledgement. So, &lt;STRONG&gt;"Bus Off"&lt;/STRONG&gt; will not happen when CANH or CANL is disconnected from the network.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Shan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jan 2018 06:13:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TJA1043-Bus-Off-is-not-detecting-CANH-or-CANL-is-open/m-p/746070#M22518</guid>
      <dc:creator>shanmugamsundar</dc:creator>
      <dc:date>2018-01-25T06:13:11Z</dc:date>
    </item>
  </channel>
</rss>