<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic The question of boot in MPC565 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/The-question-of-boot-in-MPC565/m-p/734367#M22508</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I use the CodeWarriorV8.7 without operating system to compile MPC565 boot application. The configuration is booting from inner UC3F flash which need the hardware pin "/RSTCONF" is setting to "1" and register bit "/HC" is setting to "0". I program the boot application into UC3F_A and the RCW(UC3FCFIG) into UC3F_B. The inner address base is 0x00000000. And the&amp;nbsp; RCW(UC3FCFIG) is 0x10000000.&lt;/P&gt;&lt;P&gt;Besides, I used the USB TAP to debug ROM version, and the application could run. But When power on reset happened, the MPC565 can not boot normally. I have some following quesions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. are there other hardware pins need config when MPC565 boot from inner flash?&lt;/P&gt;&lt;P&gt;2. is my RCW(UC3FCFIG) wrong?&lt;/P&gt;&lt;P&gt;3. is my program loaded into wrong place?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 19 Jan 2018 02:30:05 GMT</pubDate>
    <dc:creator>ui009123</dc:creator>
    <dc:date>2018-01-19T02:30:05Z</dc:date>
    <item>
      <title>The question of boot in MPC565</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/The-question-of-boot-in-MPC565/m-p/734367#M22508</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I use the CodeWarriorV8.7 without operating system to compile MPC565 boot application. The configuration is booting from inner UC3F flash which need the hardware pin "/RSTCONF" is setting to "1" and register bit "/HC" is setting to "0". I program the boot application into UC3F_A and the RCW(UC3FCFIG) into UC3F_B. The inner address base is 0x00000000. And the&amp;nbsp; RCW(UC3FCFIG) is 0x10000000.&lt;/P&gt;&lt;P&gt;Besides, I used the USB TAP to debug ROM version, and the application could run. But When power on reset happened, the MPC565 can not boot normally. I have some following quesions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. are there other hardware pins need config when MPC565 boot from inner flash?&lt;/P&gt;&lt;P&gt;2. is my RCW(UC3FCFIG) wrong?&lt;/P&gt;&lt;P&gt;3. is my program loaded into wrong place?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Jan 2018 02:30:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/The-question-of-boot-in-MPC565/m-p/734367#M22508</guid>
      <dc:creator>ui009123</dc:creator>
      <dc:date>2018-01-19T02:30:05Z</dc:date>
    </item>
  </channel>
</rss>