<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックBlinking across multiple PCA9745B LED drivers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Blinking-across-multiple-PCA9745B-LED-drivers/m-p/727023#M22500</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we're using two (SPI-)daisy-chained NXP &lt;A href="https://www.nxp.com/products/analog/interfaces/ic-bus/ic-general-purpose-i-o/16-channel-spi-serial-bus-57-ma-20-v-constant-current-led-driver:PCA9745B"&gt;PCA9745B LED drivers&lt;/A&gt; and want to blink some LEDs &lt;EM&gt;synchronously&lt;/EM&gt; on both ICs.&amp;nbsp; The respective LEDs of each driver are associated with a LED group that is configured identically on both ICs.&amp;nbsp; The gradation start command is issued simultaneously to both ICs.&amp;nbsp; While the LEDs on each IC are blinking in sync (as expected), the blinking frequencies&amp;nbsp;between &lt;EM&gt;different&lt;/EM&gt; ICs seem to differ and the blinking LEDs diverge pretty quickly!&amp;nbsp; I don't see any facilities for synchronizing multiple drivers (except for using the /OE pin for external dimming/blinking?)... am I missing something?&amp;nbsp; Is this use case even supported by the drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How would one go about blinking LEDs synchronously across multiple PCA9745B LED drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jan 2018 11:29:01 GMT</pubDate>
    <dc:creator>oliverebert</dc:creator>
    <dc:date>2018-01-16T11:29:01Z</dc:date>
    <item>
      <title>Blinking across multiple PCA9745B LED drivers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Blinking-across-multiple-PCA9745B-LED-drivers/m-p/727023#M22500</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we're using two (SPI-)daisy-chained NXP &lt;A href="https://www.nxp.com/products/analog/interfaces/ic-bus/ic-general-purpose-i-o/16-channel-spi-serial-bus-57-ma-20-v-constant-current-led-driver:PCA9745B"&gt;PCA9745B LED drivers&lt;/A&gt; and want to blink some LEDs &lt;EM&gt;synchronously&lt;/EM&gt; on both ICs.&amp;nbsp; The respective LEDs of each driver are associated with a LED group that is configured identically on both ICs.&amp;nbsp; The gradation start command is issued simultaneously to both ICs.&amp;nbsp; While the LEDs on each IC are blinking in sync (as expected), the blinking frequencies&amp;nbsp;between &lt;EM&gt;different&lt;/EM&gt; ICs seem to differ and the blinking LEDs diverge pretty quickly!&amp;nbsp; I don't see any facilities for synchronizing multiple drivers (except for using the /OE pin for external dimming/blinking?)... am I missing something?&amp;nbsp; Is this use case even supported by the drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How would one go about blinking LEDs synchronously across multiple PCA9745B LED drivers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and regards&lt;/P&gt;&lt;P&gt;Oliver&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 11:29:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Blinking-across-multiple-PCA9745B-LED-drivers/m-p/727023#M22500</guid>
      <dc:creator>oliverebert</dc:creator>
      <dc:date>2018-01-16T11:29:01Z</dc:date>
    </item>
    <item>
      <title>Re: Blinking across multiple PCA9745B LED drivers</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Blinking-across-multiple-PCA9745B-LED-drivers/m-p/727024#M22501</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;An FAE from our distributor confirmed that it is indeed &lt;EM&gt;not&lt;/EM&gt; possible to synchronize two or more PCA9745Bs to achieve e.g. synchronous gradation operation as described above.&amp;nbsp; This is due to the spread of the 8 MHz internal oscillator frequencies across different ICs (presumably 20--30%?), and an input for an external clock is not available.&amp;nbsp; Anyway, this seems like a missed opportunity ...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 Jan 2018 15:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Blinking-across-multiple-PCA9745B-LED-drivers/m-p/727024#M22501</guid>
      <dc:creator>oliverebert</dc:creator>
      <dc:date>2018-01-17T15:07:04Z</dc:date>
    </item>
  </channel>
</rss>