<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックHCS08 detecting LVD reset even though LVD is not enabled</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-detecting-LVD-reset-even-though-LVD-is-not-enabled/m-p/723139#M22494</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently working on MC9S08SG8 microcontroller from HCS08 family. I have disabled Low voltage detection logic with SPMSC1 = 0; and SPMSC2 = 0. But after doing power on and off sometimes I see only LVD bit in SRS register is set(POR bit is not set) . But S08 microcontroller did not go through a reset. I am not able to understand this.Can anyone please help me to understand this behaviour?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prasad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Jan 2018 07:54:43 GMT</pubDate>
    <dc:creator>prasad1</dc:creator>
    <dc:date>2018-01-15T07:54:43Z</dc:date>
    <item>
      <title>HCS08 detecting LVD reset even though LVD is not enabled</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-detecting-LVD-reset-even-though-LVD-is-not-enabled/m-p/723139#M22494</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am currently working on MC9S08SG8 microcontroller from HCS08 family. I have disabled Low voltage detection logic with SPMSC1 = 0; and SPMSC2 = 0. But after doing power on and off sometimes I see only LVD bit in SRS register is set(POR bit is not set) . But S08 microcontroller did not go through a reset. I am not able to understand this.Can anyone please help me to understand this behaviour?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Prasad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jan 2018 07:54:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-detecting-LVD-reset-even-though-LVD-is-not-enabled/m-p/723139#M22494</guid>
      <dc:creator>prasad1</dc:creator>
      <dc:date>2018-01-15T07:54:43Z</dc:date>
    </item>
    <item>
      <title>Re: HCS08 detecting LVD reset even though LVD is not enabled</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-detecting-LVD-reset-even-though-LVD-is-not-enabled/m-p/2024719#M24105</link>
      <description>&lt;P&gt;Hello, your issue is closed or not? if closed ,then what is the root cause? or anybody can help on this? I also met the same issue recently, thanks a lot~&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 09:35:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/HCS08-detecting-LVD-reset-even-though-LVD-is-not-enabled/m-p/2024719#M24105</guid>
      <dc:creator>Fidel</dc:creator>
      <dc:date>2025-01-09T09:35:20Z</dc:date>
    </item>
  </channel>
</rss>