<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollersのトピック36 to 13 pin</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/36-to-13-pin/m-p/716277#M22483</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello every body. I saw a mini ECU board that had 36 inputs. But only they use 13 pins of a micro controller. every 4 inputs goes to an optocoupler ic, every input has two pin at output, one of them connect to a diode package and the output of diode connect to micro, another connect to same pin in other optocoupler ic and then connect to a micro input pin. how it works?&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38279i4C18B2925359B2C4/image-size/large?v=v2&amp;amp;px=999" title="IMG_20180204_223432.jpg" alt="IMG_20180204_223432.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 04 Feb 2018 19:13:17 GMT</pubDate>
    <dc:creator>hosseings</dc:creator>
    <dc:date>2018-02-04T19:13:17Z</dc:date>
    <item>
      <title>36 to 13 pin</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/36-to-13-pin/m-p/716277#M22483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello every body. I saw a mini ECU board that had 36 inputs. But only they use 13 pins of a micro controller. every 4 inputs goes to an optocoupler ic, every input has two pin at output, one of them connect to a diode package and the output of diode connect to micro, another connect to same pin in other optocoupler ic and then connect to a micro input pin. how it works?&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/38279i4C18B2925359B2C4/image-size/large?v=v2&amp;amp;px=999" title="IMG_20180204_223432.jpg" alt="IMG_20180204_223432.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Feb 2018 19:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/36-to-13-pin/m-p/716277#M22483</guid>
      <dc:creator>hosseings</dc:creator>
      <dc:date>2018-02-04T19:13:17Z</dc:date>
    </item>
  </channel>
</rss>