<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックFXTH87 Flash Read/Write</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH87-Flash-Read-Write/m-p/689691#M22426</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to read and write to FLASH memory but am unable to get it working. Any help appreciated. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question&amp;nbsp;1:&amp;nbsp;How to declare a variable into FLASH?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;If I declare a variable as &lt;EM&gt;const&lt;/EM&gt;, the compiler will put the variable into FLASH. It goes to the lower part of FLASH that isn't in the "user range". If I make a custom section of the FLASH in the linker file, it will create a section of FLASH in the map. Then I can use &lt;EM&gt;#pragma&lt;/EM&gt; to designate where in FLASH the variable should be stored. The below code gets placed into 0xDDBF "TEST_ZONE" which is a 512 byte area of FLASH I have designated in the Project.prm file as a READ_WRITE area.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#pragma DATA_SEG TEST_ZONE&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; myVar3 &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;76&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#pragma DATA_SEG DEFAULT‍‍‍&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 2: How to read variable from FLASH?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;When I read a variable from&amp;nbsp;FLASH, the value is 255 no matter what I set it to. Why is that?&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;myVar3 &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;73&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;BlinkLED&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;STRONG&gt;Question 3: How to write variable to FLASH?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;In the documentation, it lays out the steps to write to FLASH. &amp;nbsp;It seems to have no effect on the values though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;FSTAT &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; FSTAT &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; 0b00010000&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN class="comment token"&gt;//Clears the flag.&lt;/SPAN&gt;
FCDIV&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;19&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Sets the Flash Clock&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;TPMS_FLASH_ERASE&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;myVar3&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//Not a pointer, but the variable itself. This returns 0 on success.&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;TPMS_FLASH_WRITE&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;‍‍‍‍&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;myVar3&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;myBuffer&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//This should replace the value at myVar with the value at myBuffer, 1 byte. It has no effect.&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 31 Jul 2017 18:01:06 GMT</pubDate>
    <dc:creator>lucascooter</dc:creator>
    <dc:date>2017-07-31T18:01:06Z</dc:date>
    <item>
      <title>FXTH87 Flash Read/Write</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH87-Flash-Read-Write/m-p/689691#M22426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to read and write to FLASH memory but am unable to get it working. Any help appreciated. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question&amp;nbsp;1:&amp;nbsp;How to declare a variable into FLASH?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;If I declare a variable as &lt;EM&gt;const&lt;/EM&gt;, the compiler will put the variable into FLASH. It goes to the lower part of FLASH that isn't in the "user range". If I make a custom section of the FLASH in the linker file, it will create a section of FLASH in the map. Then I can use &lt;EM&gt;#pragma&lt;/EM&gt; to designate where in FLASH the variable should be stored. The below code gets placed into 0xDDBF "TEST_ZONE" which is a 512 byte area of FLASH I have designated in the Project.prm file as a READ_WRITE area.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#pragma DATA_SEG TEST_ZONE&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;const&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;unsigned&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; myVar3 &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;76&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="property macro token"&gt;#pragma DATA_SEG DEFAULT‍‍‍&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Question 2: How to read variable from FLASH?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;When I read a variable from&amp;nbsp;FLASH, the value is 255 no matter what I set it to. Why is that?&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;myVar3 &lt;SPAN class="operator token"&gt;==&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;73&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;BlinkLED&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;&lt;STRONG&gt;Question 3: How to write variable to FLASH?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;In the documentation, it lays out the steps to write to FLASH. &amp;nbsp;It seems to have no effect on the values though.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;FSTAT &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; FSTAT &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt; 0b00010000&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;&amp;nbsp; &lt;SPAN class="comment token"&gt;//Clears the flag.&lt;/SPAN&gt;
FCDIV&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;19&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;// Sets the Flash Clock&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;TPMS_FLASH_ERASE&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;myVar3&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//Not a pointer, but the variable itself. This returns 0 on success.&lt;/SPAN&gt;
&lt;SPAN class="token function"&gt;TPMS_FLASH_WRITE&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;‍‍‍‍&lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;myVar3&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;myBuffer&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt; &lt;SPAN class="comment token"&gt;//This should replace the value at myVar with the value at myBuffer, 1 byte. It has no effect.&lt;/SPAN&gt;&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 31 Jul 2017 18:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/FXTH87-Flash-Read-Write/m-p/689691#M22426</guid>
      <dc:creator>lucascooter</dc:creator>
      <dc:date>2017-07-31T18:01:06Z</dc:date>
    </item>
  </channel>
</rss>