<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Changing the processor from MC9S08GT60 to MC9S08ac128 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Changing-the-processor-from-MC9S08GT60-to-MC9S08ac128/m-p/683021#M22416</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a project which had used MC9S08GT60 processor and the complete loadable file was less than 64kb.Now I changed to MC9S08ac128 processor so that we have more memory space. I am not sure whether I have to use Banked memory model or small memory model since I moved to MC9S08AC128.The code remains same. If I use banked memory model ,whether I have to do any changes specifically for banked memory model .whether the PRM file only needs to be modified .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 May 2017 23:54:04 GMT</pubDate>
    <dc:creator>preetuabraham</dc:creator>
    <dc:date>2017-05-16T23:54:04Z</dc:date>
    <item>
      <title>Changing the processor from MC9S08GT60 to MC9S08ac128</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Changing-the-processor-from-MC9S08GT60-to-MC9S08ac128/m-p/683021#M22416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on a project which had used MC9S08GT60 processor and the complete loadable file was less than 64kb.Now I changed to MC9S08ac128 processor so that we have more memory space. I am not sure whether I have to use Banked memory model or small memory model since I moved to MC9S08AC128.The code remains same. If I use banked memory model ,whether I have to do any changes specifically for banked memory model .whether the PRM file only needs to be modified .&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 May 2017 23:54:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Changing-the-processor-from-MC9S08GT60-to-MC9S08ac128/m-p/683021#M22416</guid>
      <dc:creator>preetuabraham</dc:creator>
      <dc:date>2017-05-16T23:54:04Z</dc:date>
    </item>
  </channel>
</rss>