<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックL1119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment .absSeg1</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Vector-allocated-at-absolute-address-0xFFFE-overlaps-with/m-p/680719#M22410</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm working with FXTH87 board, the example works fine (TPMS_FXTH87_LF_RF_Communication) in this example redefine the Vector Interrupts table in a Interrupts.c.&lt;/P&gt;&lt;P&gt;But when i try to create a new project and do the same the compiler show&amp;nbsp;L1119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment .absSeg1, this error is because i redefine the Vector Interrupts Table but How I can solve my problem for not show this Error.&lt;/P&gt;&lt;P&gt;#include "derivative.h"&lt;BR /&gt;#include "main.h" /* Reference to FrameID and RF_Interrupt */&lt;/P&gt;&lt;P&gt;/* SWI Interrupt */&lt;BR /&gt;void interrupt USER_1_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* RESERVED - Don't use */&lt;BR /&gt;void interrupt USER_2_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* LVD Interrupt */&lt;BR /&gt;void interrupt USER_3_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* PWU Interrupt */&lt;BR /&gt;void interrupt USER_4_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt; &lt;BR /&gt; /* Clear all PWU Interrupt flags */&lt;BR /&gt; PWUCS0_WUFACK = SET;&lt;BR /&gt; PWUCS1_PRFACK = SET;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;/* TPM1CH0 Interrupt */&lt;BR /&gt;void interrupt USER_5_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* TPM1CH1 Interrupt */&lt;BR /&gt;void interrupt USER_6_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* TPM1 Interrupt */&lt;BR /&gt;void interrupt USER_7_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* SMI Interrupt - Don't use */&lt;BR /&gt;void interrupt USER_8_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* RFM Interrupt */&lt;BR /&gt;void interrupt USER_9_INTERRUPT(void)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;RFCR7_RFIACK = SET;&lt;BR /&gt; FrameID++;&lt;BR /&gt; RF_Interrupt = SET;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;/* ADC Interrupt - Don't use */&lt;BR /&gt;void interrupt USER_10_INTERRUPT(void)&lt;BR /&gt;{ &lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* LFR Interrupt */&lt;BR /&gt;void interrupt USER_11_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt; LFS_LFIACK = SET;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;/* RTI Interrupt */&lt;BR /&gt;void interrupt USER_12_INTERRUPT(void)&lt;BR /&gt;{ &lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* RESERVED - Don't use */&lt;BR /&gt;void interrupt USER_13_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* RESERVED - Don't use */&lt;BR /&gt;void interrupt USER_14_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* KBI Interrupt */&lt;BR /&gt;void interrupt USER_15_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt; //A valid edge or level on an enabled KBI pin will set KBF in KBISC. If KBIE in KBISC is set, an interrupt request will be presented&lt;BR /&gt; //to the CPU. Clearing of KBF is accomplished by writing a 1 to KBACK in KBISC provided all enabled keyboard inputs are at their&lt;BR /&gt; //reset levels. KBF will remain set if any enabled KBI pin is asserted while attempting to clear by writing a 1 to KBACK.&lt;BR /&gt; KBISC_KBACK = SET;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void(* const USER_INTERRUPT_TABLE[])() @ 0xDFE0 =&lt;BR /&gt;{&lt;BR /&gt; USER_15_INTERRUPT,&lt;BR /&gt; USER_14_INTERRUPT,&lt;BR /&gt; USER_13_INTERRUPT,&lt;BR /&gt; USER_12_INTERRUPT,&lt;BR /&gt; USER_11_INTERRUPT,&lt;BR /&gt; USER_10_INTERRUPT,&lt;BR /&gt; USER_9_INTERRUPT,&lt;BR /&gt; USER_8_INTERRUPT,&lt;BR /&gt; USER_7_INTERRUPT,&lt;BR /&gt; USER_6_INTERRUPT,&lt;BR /&gt; USER_5_INTERRUPT,&lt;BR /&gt; USER_4_INTERRUPT,&lt;BR /&gt; USER_3_INTERRUPT,&lt;BR /&gt; USER_2_INTERRUPT,&lt;BR /&gt; USER_1_INTERRUPT,&lt;BR /&gt; main&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 May 2017 22:03:47 GMT</pubDate>
    <dc:creator>davidramirez</dc:creator>
    <dc:date>2017-05-15T22:03:47Z</dc:date>
    <item>
      <title>L1119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment .absSeg1</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Vector-allocated-at-absolute-address-0xFFFE-overlaps-with/m-p/680719#M22410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm working with FXTH87 board, the example works fine (TPMS_FXTH87_LF_RF_Communication) in this example redefine the Vector Interrupts table in a Interrupts.c.&lt;/P&gt;&lt;P&gt;But when i try to create a new project and do the same the compiler show&amp;nbsp;L1119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment .absSeg1, this error is because i redefine the Vector Interrupts Table but How I can solve my problem for not show this Error.&lt;/P&gt;&lt;P&gt;#include "derivative.h"&lt;BR /&gt;#include "main.h" /* Reference to FrameID and RF_Interrupt */&lt;/P&gt;&lt;P&gt;/* SWI Interrupt */&lt;BR /&gt;void interrupt USER_1_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* RESERVED - Don't use */&lt;BR /&gt;void interrupt USER_2_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* LVD Interrupt */&lt;BR /&gt;void interrupt USER_3_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* PWU Interrupt */&lt;BR /&gt;void interrupt USER_4_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt; &lt;BR /&gt; /* Clear all PWU Interrupt flags */&lt;BR /&gt; PWUCS0_WUFACK = SET;&lt;BR /&gt; PWUCS1_PRFACK = SET;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;/* TPM1CH0 Interrupt */&lt;BR /&gt;void interrupt USER_5_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* TPM1CH1 Interrupt */&lt;BR /&gt;void interrupt USER_6_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* TPM1 Interrupt */&lt;BR /&gt;void interrupt USER_7_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* SMI Interrupt - Don't use */&lt;BR /&gt;void interrupt USER_8_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* RFM Interrupt */&lt;BR /&gt;void interrupt USER_9_INTERRUPT(void)&lt;BR /&gt;{&lt;/P&gt;&lt;P&gt;RFCR7_RFIACK = SET;&lt;BR /&gt; FrameID++;&lt;BR /&gt; RF_Interrupt = SET;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;/* ADC Interrupt - Don't use */&lt;BR /&gt;void interrupt USER_10_INTERRUPT(void)&lt;BR /&gt;{ &lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* LFR Interrupt */&lt;BR /&gt;void interrupt USER_11_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt; LFS_LFIACK = SET;&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;/* RTI Interrupt */&lt;BR /&gt;void interrupt USER_12_INTERRUPT(void)&lt;BR /&gt;{ &lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* RESERVED - Don't use */&lt;BR /&gt;void interrupt USER_13_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* RESERVED - Don't use */&lt;BR /&gt;void interrupt USER_14_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;/* KBI Interrupt */&lt;BR /&gt;void interrupt USER_15_INTERRUPT(void)&lt;BR /&gt;{&lt;BR /&gt; //A valid edge or level on an enabled KBI pin will set KBF in KBISC. If KBIE in KBISC is set, an interrupt request will be presented&lt;BR /&gt; //to the CPU. Clearing of KBF is accomplished by writing a 1 to KBACK in KBISC provided all enabled keyboard inputs are at their&lt;BR /&gt; //reset levels. KBF will remain set if any enabled KBI pin is asserted while attempting to clear by writing a 1 to KBACK.&lt;BR /&gt; KBISC_KBACK = SET;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;void(* const USER_INTERRUPT_TABLE[])() @ 0xDFE0 =&lt;BR /&gt;{&lt;BR /&gt; USER_15_INTERRUPT,&lt;BR /&gt; USER_14_INTERRUPT,&lt;BR /&gt; USER_13_INTERRUPT,&lt;BR /&gt; USER_12_INTERRUPT,&lt;BR /&gt; USER_11_INTERRUPT,&lt;BR /&gt; USER_10_INTERRUPT,&lt;BR /&gt; USER_9_INTERRUPT,&lt;BR /&gt; USER_8_INTERRUPT,&lt;BR /&gt; USER_7_INTERRUPT,&lt;BR /&gt; USER_6_INTERRUPT,&lt;BR /&gt; USER_5_INTERRUPT,&lt;BR /&gt; USER_4_INTERRUPT,&lt;BR /&gt; USER_3_INTERRUPT,&lt;BR /&gt; USER_2_INTERRUPT,&lt;BR /&gt; USER_1_INTERRUPT,&lt;BR /&gt; main&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 May 2017 22:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Vector-allocated-at-absolute-address-0xFFFE-overlaps-with/m-p/680719#M22410</guid>
      <dc:creator>davidramirez</dc:creator>
      <dc:date>2017-05-15T22:03:47Z</dc:date>
    </item>
    <item>
      <title>Re: L1119: Vector allocated at absolute address 0xFFFE overlaps with sections placed in segment .absSeg1</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Vector-allocated-at-absolute-address-0xFFFE-overlaps-with/m-p/680720#M22411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found my error, In th proyect in linker files I modify Project.prm Start direcction and Found my Project.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 17 May 2017 13:30:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/L1119-Vector-allocated-at-absolute-address-0xFFFE-overlaps-with/m-p/680720#M22411</guid>
      <dc:creator>davidramirez</dc:creator>
      <dc:date>2017-05-17T13:30:01Z</dc:date>
    </item>
  </channel>
</rss>