<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Relative values of A2D Input Leakage Currents</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Relative-values-of-A2D-Input-Leakage-Currents/m-p/677288#M22405</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-top: 0pt; margin-bottom: 0pt; margin-left: 0in; text-indent: 0in;"&gt;&lt;SPAN style="font-size: 11.0pt; color: black;"&gt;The S9S08RNA16W2MLCR A2D data sheet specifies the range of input pin leakage currents as&amp;nbsp; -1uA to +1uA. &amp;nbsp;I have high impedance series input resistors (500Kohm to 1MHom) to a pair of analog signals the connect to two microcontroller A2D input pins.&amp;nbsp;&amp;nbsp; Can I assume that the leakage currents of the two A2D input pins will match if the input voltage are the same?&amp;nbsp; That is, if one pin leaks 1uA , will the other pin leak 1uA as well if both input voltage are the same?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 20 Jul 2017 12:29:22 GMT</pubDate>
    <dc:creator>stephenwhite</dc:creator>
    <dc:date>2017-07-20T12:29:22Z</dc:date>
    <item>
      <title>Relative values of A2D Input Leakage Currents</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Relative-values-of-A2D-Input-Leakage-Currents/m-p/677288#M22405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="margin-top: 0pt; margin-bottom: 0pt; margin-left: 0in; text-indent: 0in;"&gt;&lt;SPAN style="font-size: 11.0pt; color: black;"&gt;The S9S08RNA16W2MLCR A2D data sheet specifies the range of input pin leakage currents as&amp;nbsp; -1uA to +1uA. &amp;nbsp;I have high impedance series input resistors (500Kohm to 1MHom) to a pair of analog signals the connect to two microcontroller A2D input pins.&amp;nbsp;&amp;nbsp; Can I assume that the leakage currents of the two A2D input pins will match if the input voltage are the same?&amp;nbsp; That is, if one pin leaks 1uA , will the other pin leak 1uA as well if both input voltage are the same?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 20 Jul 2017 12:29:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Relative-values-of-A2D-Input-Leakage-Currents/m-p/677288#M22405</guid>
      <dc:creator>stephenwhite</dc:creator>
      <dc:date>2017-07-20T12:29:22Z</dc:date>
    </item>
  </channel>
</rss>