<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value. in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662973#M22363</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Normally the device after reset set the ICS to use the internal clock, (FEI), so probably your device is running with the internal clock, you can check it debuging the ICS register using code warrior.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Nov 2016 17:24:09 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2016-11-28T17:24:09Z</dc:date>
    <item>
      <title>RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662970#M22360</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using extern 5MHz clock, set bus to 10MHz, When I use RDIV other than&amp;nbsp;divide 128, MCU work the same.&lt;/P&gt;&lt;P&gt;Strange, is it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Oct 2016 06:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662970#M22360</guid>
      <dc:creator>w_tension</dc:creator>
      <dc:date>2016-10-24T06:49:21Z</dc:date>
    </item>
    <item>
      <title>Re: RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662971#M22361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Are you sure that the MCU is running with the external clock?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Nov 2016 19:27:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662971#M22361</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-11-17T19:27:18Z</dc:date>
    </item>
    <item>
      <title>Re: RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662972#M22362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Not quite sure. Just find serial communication still working.&lt;/P&gt;&lt;P&gt;UM doesn't mention what happens when a abnormal value is used.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 14:16:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662972#M22362</guid>
      <dc:creator>w_tension</dc:creator>
      <dc:date>2016-11-28T14:16:33Z</dc:date>
    </item>
    <item>
      <title>Re: RS08, When ICS uses a wrong RDIV value, MCU works the same as with a right value.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662973#M22363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Normally the device after reset set the ICS to use the internal clock, (FEI), so probably your device is running with the internal clock, you can check it debuging the ICS register using code warrior.&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 17:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/RS08-When-ICS-uses-a-wrong-RDIV-value-MCU-works-the-same-as-with/m-p/662973#M22363</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-11-28T17:24:09Z</dc:date>
    </item>
  </channel>
</rss>