<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックTimer and sleep behavior: debugger vs no debugger</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Timer-and-sleep-behavior-debugger-vs-no-debugger/m-p/660189#M22351</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the MC13234, I'm seeing some weird inconsistencies in timer and sleep behavior between when I download the code and have the debugger attached, and when the debugger is not attached and the code is running freely. I'm interested if anyone could give me some tips or point me toward an application note that explains the differences in how the timers and STOP3 mode might work with and without the debugger attached, so I can track down the source of the discrepancy and find a workaround.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 May 2017 16:43:27 GMT</pubDate>
    <dc:creator>matthammond</dc:creator>
    <dc:date>2017-05-03T16:43:27Z</dc:date>
    <item>
      <title>Timer and sleep behavior: debugger vs no debugger</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Timer-and-sleep-behavior-debugger-vs-no-debugger/m-p/660189#M22351</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;On the MC13234, I'm seeing some weird inconsistencies in timer and sleep behavior between when I download the code and have the debugger attached, and when the debugger is not attached and the code is running freely. I'm interested if anyone could give me some tips or point me toward an application note that explains the differences in how the timers and STOP3 mode might work with and without the debugger attached, so I can track down the source of the discrepancy and find a workaround.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 May 2017 16:43:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Timer-and-sleep-behavior-debugger-vs-no-debugger/m-p/660189#M22351</guid>
      <dc:creator>matthammond</dc:creator>
      <dc:date>2017-05-03T16:43:27Z</dc:date>
    </item>
  </channel>
</rss>