<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: what is the best programmer for S08 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650821#M22308</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You might look at Tag-Connect. They don't have a cable specifically branded for NXP but you could easily make an adapter. With these you don't need a connector at all, just pads on the board (or pads and holes if you want to use it for debug as well and leave the connector attached). I have used these with several parts from other manufacturers with 100% success. &lt;A class="link-titled" href="http://www.tag-connect.com/what-is-tag-connect" title="http://www.tag-connect.com/what-is-tag-connect"&gt;What is Tag Connect? - Tag Connect&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Mar 2017 15:44:04 GMT</pubDate>
    <dc:creator>bpedm</dc:creator>
    <dc:date>2017-03-30T15:44:04Z</dc:date>
    <item>
      <title>what is the best programmer for S08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650819#M22306</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Continuing my learning curve in migrating from LPC900 to S08, I need to debug a new design and subsequently program the first 100 production units. My problem is space. I will be using a DEMOQE board + proto board for functional design and test and a Freescale USBDM pod for testing the prototype PCB. This board can easily accommodate the 6-pin BDM header, but space is a MAJOR problem for the production boards. What is the minimum (smallest) interface needed for programming? Pre-programming the chips is not an option as there may be subsequent changes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2017 12:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650819#M22306</guid>
      <dc:creator>juliancox</dc:creator>
      <dc:date>2017-03-14T12:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: what is the best programmer for S08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650820#M22307</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I don't know if this will solve your problem, but I just finished a product design of a handheld device that uses (2) S08 processors on board.&amp;nbsp; I kep all (6) pins of the BDM interface but used a 50-mil pitch lower profile female (socket) part.&lt;/P&gt;&lt;P&gt;SAMTEC .050" pitch 6 pos female socket&amp;nbsp; P/N&amp;nbsp;&amp;nbsp; CLP-103-02-G-D&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We then just made up some small adapter PCBs (postage-stamp sized) to convert the 100mil pitch 6 way male header that mates with the typically .100" square ribbon cable connector from the PE Micro programmers&amp;nbsp; to the 50mil pitch mating SAMTEC header to plug into the PCB.&amp;nbsp;&amp;nbsp; I can basically fit the (2) programming/debug connectors on the PCB in the same real estate as (1) of the "standard" .100" 6 pos BDM header, and much less than half the height (which was a big issue for me).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Mar 2017 15:13:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650820#M22307</guid>
      <dc:creator>mfugere</dc:creator>
      <dc:date>2017-03-14T15:13:22Z</dc:date>
    </item>
    <item>
      <title>Re: what is the best programmer for S08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650821#M22308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You might look at Tag-Connect. They don't have a cable specifically branded for NXP but you could easily make an adapter. With these you don't need a connector at all, just pads on the board (or pads and holes if you want to use it for debug as well and leave the connector attached). I have used these with several parts from other manufacturers with 100% success. &lt;A class="link-titled" href="http://www.tag-connect.com/what-is-tag-connect" title="http://www.tag-connect.com/what-is-tag-connect"&gt;What is Tag Connect? - Tag Connect&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Mar 2017 15:44:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650821#M22308</guid>
      <dc:creator>bpedm</dc:creator>
      <dc:date>2017-03-30T15:44:04Z</dc:date>
    </item>
    <item>
      <title>Re: what is the best programmer for S08</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650822#M22309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I have successfully used&amp;nbsp; 4 pins to debug and connect a 9S08 series micro controller.&amp;nbsp; Those are RESET, BKGD, Gnd, Vcc. I have also changed the connector to a 4 pin with 2mm spacing and so far had more then a thousand units programmed with minor glitches ( production decided to use the same connector to power the target PCB as well &amp;amp; fried the P&amp;amp;E Multilink by mistakenly connecting +12V ). The target PCB actually only has a dedicated spot for connecting to the programmer - the header or socket is usually not soldered there.&amp;nbsp; The connection cable is terminated with 4 male pins which just plug into the holes on the PCB. Such a connection needs to be secured by hand, which is not a problem since the whole operation lasts less then 10 seconds. The price is 2mm x 10mm area on both sides of the board - since the 4 holes are metalized, and a doctored P&amp;amp;E cable which has to be rebuild once every two years.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Apr 2017 21:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/what-is-the-best-programmer-for-S08/m-p/650822#M22309</guid>
      <dc:creator>KrisRutecki</dc:creator>
      <dc:date>2017-04-06T21:17:00Z</dc:date>
    </item>
  </channel>
</rss>