<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic mc68hc908ap32 Monitor Mode Debugging in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908ap32-Monitor-Mode-Debugging/m-p/619277#M22222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, how i can exit monitor MODE and run code IN user MODE without POR (eq. power-of-reset)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I trying save stack&amp;amp;RAM variables which wrote while MCU in monitor mode, and start user code in user mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to create little subroutine for debugging MCU in Monitor mode. I read an2295 but i don't want to use this way because need to re-burn MCU with bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(sorry for my English)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I not fully understand what is exactly Monitor mode - this is some special kind of interrupt or subroutine and i can return to user mode with my variables etc. or this is some hardware module, and i can't do any actions (beside hardware) to back in user mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 04 Mar 2017 10:29:24 GMT</pubDate>
    <dc:creator>kuraga200</dc:creator>
    <dc:date>2017-03-04T10:29:24Z</dc:date>
    <item>
      <title>mc68hc908ap32 Monitor Mode Debugging</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908ap32-Monitor-Mode-Debugging/m-p/619277#M22222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, how i can exit monitor MODE and run code IN user MODE without POR (eq. power-of-reset)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I trying save stack&amp;amp;RAM variables which wrote while MCU in monitor mode, and start user code in user mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I try to create little subroutine for debugging MCU in Monitor mode. I read an2295 but i don't want to use this way because need to re-burn MCU with bootloader.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(sorry for my English)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I not fully understand what is exactly Monitor mode - this is some special kind of interrupt or subroutine and i can return to user mode with my variables etc. or this is some hardware module, and i can't do any actions (beside hardware) to back in user mode.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 04 Mar 2017 10:29:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/mc68hc908ap32-Monitor-Mode-Debugging/m-p/619277#M22222</guid>
      <dc:creator>kuraga200</dc:creator>
      <dc:date>2017-03-04T10:29:24Z</dc:date>
    </item>
  </channel>
</rss>