<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Bootloader jump to application，some of application‘s function error in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-jump-to-application-some-of-application-s-function/m-p/618606#M22220</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the reason, in bootloader and application use different communication protocols, in application, the CAN reinitialization doesnt work, so I set the CANCTL0 = 0x01,then jump to application, it works as expected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Dec 2016 05:59:07 GMT</pubDate>
    <dc:creator>zonglinyao</dc:creator>
    <dc:date>2016-12-05T05:59:07Z</dc:date>
    <item>
      <title>Bootloader jump to application，some of application‘s function error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-jump-to-application-some-of-application-s-function/m-p/618605#M22219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone，please forgive me for my poor English.&lt;/P&gt;&lt;P&gt;In MC9S08DZ60, I wrote a bootloader in case to upgrade my application, now I met a problem. In my bootloader, if no upgrade signal received from CAN-BUS, then jump to application. When jumpped to application, some functions could not execute, e.g. I send &amp;nbsp;commands via CAN-BUS to application, some commands have right response, but others no.&lt;/P&gt;&lt;P&gt;I don't understand why? &amp;nbsp;If only program application into flash, it running normally.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Could anybody help me?&lt;/P&gt;&lt;P&gt;Best Regards!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Nov 2016 10:42:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-jump-to-application-some-of-application-s-function/m-p/618605#M22219</guid>
      <dc:creator>zonglinyao</dc:creator>
      <dc:date>2016-11-23T10:42:27Z</dc:date>
    </item>
    <item>
      <title>Re: Bootloader jump to application，some of application‘s function error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-jump-to-application-some-of-application-s-function/m-p/618606#M22220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I found the reason, in bootloader and application use different communication protocols, in application, the CAN reinitialization doesnt work, so I set the CANCTL0 = 0x01,then jump to application, it works as expected.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Dec 2016 05:59:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Bootloader-jump-to-application-some-of-application-s-function/m-p/618606#M22220</guid>
      <dc:creator>zonglinyao</dc:creator>
      <dc:date>2016-12-05T05:59:07Z</dc:date>
    </item>
  </channel>
</rss>