<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックENGR00286342 (The Target Task (Flash file to Target) does not program S19 files into MC13237)</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ENGR00286342-The-Target-Task-Flash-file-to-Target-does-not/m-p/616189#M22211</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm reviewing the release notes for Codewarrior for MCUs v10.6 and there is, what seems to be, an important note about the MC13237, which I don't understand. See the cut &amp;amp; paste below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I searched through Codewarrior and cannot find the "Flash File to Target" dialog. Can someone get me to this first step?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ENGR00286342&lt;BR /&gt;Description: The Target Task (Flash file to Target) does not into MC13237.&lt;BR /&gt;Workaround: The default "Flash File to Target" task can be remove restricted areas. The following actions are required:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Select "Save as Target Task" in the “Flash File to Target” dialog&lt;BR /&gt;- Specify task name&lt;BR /&gt;- Perform Erase and Program&lt;BR /&gt;- In the dialog “Save Resource” specify the path&lt;BR /&gt;- Open the Target Tasks tab&lt;BR /&gt;- Select the saved task&lt;BR /&gt;- Select “Edit task Configuration” from local menu&lt;BR /&gt;- Double click on Erase and Program operations in the list of Flash Programmer actions&lt;BR /&gt;- “Add Program/Verify Action” dialog will open&lt;BR /&gt;- Uncheck "Restrict to Addresses in this Range"&lt;BR /&gt;- Close dialog with “Update Program Action” button.&lt;BR /&gt;Now use this task to flash the S19 files into MC13237&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Mar 2017 15:55:55 GMT</pubDate>
    <dc:creator>markthedark</dc:creator>
    <dc:date>2017-03-02T15:55:55Z</dc:date>
    <item>
      <title>ENGR00286342 (The Target Task (Flash file to Target) does not program S19 files into MC13237)</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ENGR00286342-The-Target-Task-Flash-file-to-Target-does-not/m-p/616189#M22211</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm reviewing the release notes for Codewarrior for MCUs v10.6 and there is, what seems to be, an important note about the MC13237, which I don't understand. See the cut &amp;amp; paste below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I searched through Codewarrior and cannot find the "Flash File to Target" dialog. Can someone get me to this first step?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Mark&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;ENGR00286342&lt;BR /&gt;Description: The Target Task (Flash file to Target) does not into MC13237.&lt;BR /&gt;Workaround: The default "Flash File to Target" task can be remove restricted areas. The following actions are required:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- Select "Save as Target Task" in the “Flash File to Target” dialog&lt;BR /&gt;- Specify task name&lt;BR /&gt;- Perform Erase and Program&lt;BR /&gt;- In the dialog “Save Resource” specify the path&lt;BR /&gt;- Open the Target Tasks tab&lt;BR /&gt;- Select the saved task&lt;BR /&gt;- Select “Edit task Configuration” from local menu&lt;BR /&gt;- Double click on Erase and Program operations in the list of Flash Programmer actions&lt;BR /&gt;- “Add Program/Verify Action” dialog will open&lt;BR /&gt;- Uncheck "Restrict to Addresses in this Range"&lt;BR /&gt;- Close dialog with “Update Program Action” button.&lt;BR /&gt;Now use this task to flash the S19 files into MC13237&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Mar 2017 15:55:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ENGR00286342-The-Target-Task-Flash-file-to-Target-does-not/m-p/616189#M22211</guid>
      <dc:creator>markthedark</dc:creator>
      <dc:date>2017-03-02T15:55:55Z</dc:date>
    </item>
  </channel>
</rss>