<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックParallel programming 89c668</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Parallel-programming-89c668/m-p/606056#M22186</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I would like to program P89C668 microcontroller&amp;nbsp;using parallel programming method.&amp;nbsp;I have almost every information, but I need some details. I know which pins act as address llines (A0-A15) for flashing, but the available resources said the status byte and boot vector&amp;nbsp;can be programmed at address 10000 hex &amp;nbsp;and &amp;nbsp;10001 hex. It means I&amp;nbsp;have to use A16, &amp;nbsp;but I do not know which pin has to be used for this address.&lt;/P&gt;&lt;P&gt;My&amp;nbsp;second question is the method to erasing the chip using parallel programming technic.&lt;/P&gt;&lt;P&gt;The answer for the first question is the most important to me, because after set boot vector back to the factory default &amp;nbsp;I will be able to erase and program the chip using ISP method.&lt;/P&gt;&lt;P&gt;Help me please if you know the answer. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Sep 2016 16:46:33 GMT</pubDate>
    <dc:creator>attilagallai</dc:creator>
    <dc:date>2016-09-09T16:46:33Z</dc:date>
    <item>
      <title>Parallel programming 89c668</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Parallel-programming-89c668/m-p/606056#M22186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P&gt;I would like to program P89C668 microcontroller&amp;nbsp;using parallel programming method.&amp;nbsp;I have almost every information, but I need some details. I know which pins act as address llines (A0-A15) for flashing, but the available resources said the status byte and boot vector&amp;nbsp;can be programmed at address 10000 hex &amp;nbsp;and &amp;nbsp;10001 hex. It means I&amp;nbsp;have to use A16, &amp;nbsp;but I do not know which pin has to be used for this address.&lt;/P&gt;&lt;P&gt;My&amp;nbsp;second question is the method to erasing the chip using parallel programming technic.&lt;/P&gt;&lt;P&gt;The answer for the first question is the most important to me, because after set boot vector back to the factory default &amp;nbsp;I will be able to erase and program the chip using ISP method.&lt;/P&gt;&lt;P&gt;Help me please if you know the answer. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2016 16:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Parallel-programming-89c668/m-p/606056#M22186</guid>
      <dc:creator>attilagallai</dc:creator>
      <dc:date>2016-09-09T16:46:33Z</dc:date>
    </item>
  </channel>
</rss>