<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic 9S08AC60 Reset Levels in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-Reset-Levels/m-p/597531#M22161</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my end-user application/product, I need the ability for a "master" MC9S08AC60CPUE to be able to reset a "slave" MC9S08AC60CPUE , while still allowing for pod debug &amp;amp; production programming of the "slave" regardless of the state of the master.&amp;nbsp; To do this inexpensively, I am using a series resistor from a Master's I/O pin to the slave's reset pin, and slave's reset pin is also connected to the debug pod connector on the PCB.&amp;nbsp; The reset pin on the slave presently has no externally added pullup, but does have 100nF filter cap to GND.&amp;nbsp; The internal pullup on the reset pin appears to be approximately 30K, as with a series resistance of 5K to the Master's I/O pin, it can only maintain a low voltage of 0.7V, which I think may not be reliably resetting the slave.&amp;nbsp;&amp;nbsp; If I lower series resistance to 2.7K, it can maintain a low level of approximately 0.38V.&lt;/P&gt;&lt;P&gt;The MC9S08AC60 datasheet indicates a maximum low voltage input level of 0.35xVdd which would yield&amp;nbsp; 1.75V in my application, but I think the reset line must go significantly lower than that to ensure reset.&amp;nbsp; I don't want to go too low in series resistance and then have problems with the programming pod current limit.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, what levels of voltage are necessary on the dedicated Reset Pin to ensure the micro is held in reset state?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Dec 2016 14:45:04 GMT</pubDate>
    <dc:creator>mfugere</dc:creator>
    <dc:date>2016-12-09T14:45:04Z</dc:date>
    <item>
      <title>9S08AC60 Reset Levels</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-Reset-Levels/m-p/597531#M22161</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my end-user application/product, I need the ability for a "master" MC9S08AC60CPUE to be able to reset a "slave" MC9S08AC60CPUE , while still allowing for pod debug &amp;amp; production programming of the "slave" regardless of the state of the master.&amp;nbsp; To do this inexpensively, I am using a series resistor from a Master's I/O pin to the slave's reset pin, and slave's reset pin is also connected to the debug pod connector on the PCB.&amp;nbsp; The reset pin on the slave presently has no externally added pullup, but does have 100nF filter cap to GND.&amp;nbsp; The internal pullup on the reset pin appears to be approximately 30K, as with a series resistance of 5K to the Master's I/O pin, it can only maintain a low voltage of 0.7V, which I think may not be reliably resetting the slave.&amp;nbsp;&amp;nbsp; If I lower series resistance to 2.7K, it can maintain a low level of approximately 0.38V.&lt;/P&gt;&lt;P&gt;The MC9S08AC60 datasheet indicates a maximum low voltage input level of 0.35xVdd which would yield&amp;nbsp; 1.75V in my application, but I think the reset line must go significantly lower than that to ensure reset.&amp;nbsp; I don't want to go too low in series resistance and then have problems with the programming pod current limit.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, what levels of voltage are necessary on the dedicated Reset Pin to ensure the micro is held in reset state?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 14:45:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/9S08AC60-Reset-Levels/m-p/597531#M22161</guid>
      <dc:creator>mfugere</dc:creator>
      <dc:date>2016-12-09T14:45:04Z</dc:date>
    </item>
  </channel>
</rss>