<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックDependency between S08RN's ICS_C3 register and the internal trimmed oscillator</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Dependency-between-S08RN-s-ICS-C3-register-and-the-internal/m-p/579645#M22121</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;What is the direct dependency between the ICS_C3 value from the register and the internal trimmed oscillator ? &lt;/P&gt;&lt;P&gt;How much is the frequency decreased with 1 increment in that register (best case and worst case) ?&lt;/P&gt;&lt;P&gt;I searched through application notes and the datasheet for S08RN microcontrollers and I couldn't find a specific value.&lt;/P&gt;&lt;P&gt;I need this figure in order to be able to calculate that I can reach a certain accuracy with the system oscillator.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jun 2016 10:30:48 GMT</pubDate>
    <dc:creator>cristianstancu</dc:creator>
    <dc:date>2016-06-28T10:30:48Z</dc:date>
    <item>
      <title>Dependency between S08RN's ICS_C3 register and the internal trimmed oscillator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Dependency-between-S08RN-s-ICS-C3-register-and-the-internal/m-p/579645#M22121</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;What is the direct dependency between the ICS_C3 value from the register and the internal trimmed oscillator ? &lt;/P&gt;&lt;P&gt;How much is the frequency decreased with 1 increment in that register (best case and worst case) ?&lt;/P&gt;&lt;P&gt;I searched through application notes and the datasheet for S08RN microcontrollers and I couldn't find a specific value.&lt;/P&gt;&lt;P&gt;I need this figure in order to be able to calculate that I can reach a certain accuracy with the system oscillator.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jun 2016 10:30:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Dependency-between-S08RN-s-ICS-C3-register-and-the-internal/m-p/579645#M22121</guid>
      <dc:creator>cristianstancu</dc:creator>
      <dc:date>2016-06-28T10:30:48Z</dc:date>
    </item>
    <item>
      <title>Re: Dependency between S08RN's ICS_C3 register and the internal trimmed oscillator</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Dependency-between-S08RN-s-ICS-C3-register-and-the-internal/m-p/579646#M22122</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Cristian&lt;/P&gt;&lt;P&gt;I check it using PE on the S08PT ( I do not have the S08RN) and with 0x81 on ICS_C3&amp;nbsp; I got 31.25&amp;nbsp; KHz also you need to check the ICS_C4 due the fine trim is on that register. for this case ICS_C4 was 0&lt;/P&gt;&lt;P&gt;But while I was testing different value on the ICS_C3 I saw that this is no lineal, so I can not give you an spec for that.&lt;/P&gt;&lt;P&gt;Some data that I got was 39 KHz ICS_C3 = 0x43 ICS_C4 = 0&lt;/P&gt;&lt;P&gt; 39 KHz ICS_C3 = 0x43 ICS_C4 = 0&lt;/P&gt;&lt;P&gt;31.50 KhZ&amp;nbsp; ICS_C3 = 0x7E ICS_C4 = 0x00&lt;/P&gt;&lt;P&gt;31.45 KhZ&amp;nbsp; ICS_C3 = 0x7E ICS_C4 = 0x01&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note I also was using the ciclone pro to debug the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jun 2016 22:00:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Dependency-between-S08RN-s-ICS-C3-register-and-the-internal/m-p/579646#M22122</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-06-30T22:00:53Z</dc:date>
    </item>
  </channel>
</rss>