<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: ICS Factory Trimming</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICS-Factory-Trimming/m-p/577234#M22120</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;please also check this application note for more information about the ICS and the clock option on the S08&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN3499.pdf?fsrch=1&amp;amp;sr=3&amp;amp;pageNum=1"&gt;Clock Options on the HC9S08 Family&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Sep 2016 17:23:17 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2016-09-05T17:23:17Z</dc:date>
    <item>
      <title>ICS Factory Trimming</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICS-Factory-Trimming/m-p/577232#M22118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I want to work with the factory trimming values but, as&amp;nbsp;far as i understand, those values are not loaded into the ICS trim registers if BDM is active.&lt;/P&gt;&lt;P&gt;This means that during development, while i am&amp;nbsp;working with a debugger, i&amp;nbsp;can not get the device to run with the factory trim values.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a way to read and load the factory trim values into the ICS trim registers?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am working with CW10.6, MC9S08PA8, P&amp;amp;E Multilink debugger&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Timor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 06:55:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICS-Factory-Trimming/m-p/577232#M22118</guid>
      <dc:creator>Timor</dc:creator>
      <dc:date>2016-08-31T06:55:39Z</dc:date>
    </item>
    <item>
      <title>Re: ICS Factory Trimming</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICS-Factory-Trimming/m-p/577233#M22119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CodeWarrior load the TRIM value by default when debug, and it's optional, you can turn off.&lt;/P&gt;&lt;P&gt;User should load by himself, example projects do this, too.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="QQ截图20160901090221.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/2812iF3640E7FC480C811/image-size/large?v=v2&amp;amp;px=999" role="button" title="QQ截图20160901090221.png" alt="QQ截图20160901090221.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Sep 2016 01:03:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICS-Factory-Trimming/m-p/577233#M22119</guid>
      <dc:creator>w_tension</dc:creator>
      <dc:date>2016-09-01T01:03:19Z</dc:date>
    </item>
    <item>
      <title>Re: ICS Factory Trimming</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/ICS-Factory-Trimming/m-p/577234#M22120</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;please also check this application note for more information about the ICS and the clock option on the S08&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN3499.pdf?fsrch=1&amp;amp;sr=3&amp;amp;pageNum=1"&gt;Clock Options on the HC9S08 Family&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Sep 2016 17:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/ICS-Factory-Trimming/m-p/577234#M22120</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-09-05T17:23:17Z</dc:date>
    </item>
  </channel>
</rss>