<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックInput Capture of MC68HC908JK3E</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Input-Capture-of-MC68HC908JK3E/m-p/576948#M22113</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the chip is MC68HC908JK3E, select the timer's channel 1 to capture the external input square wave signal (100-250Hz) period. At the same time, according to the different period, I use timer's channel 0 output adjustable duty cycle square wave signal (20KHz). In the program, I constantly modify the TCH0H and TCH0L to change the duty cycle of the output signal. The current problems are: the capture signal cycle is not accurate, what are the reasons for this? Thank you!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337726"&gt;code.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Aug 2016 09:05:07 GMT</pubDate>
    <dc:creator>peakgao</dc:creator>
    <dc:date>2016-08-31T09:05:07Z</dc:date>
    <item>
      <title>Input Capture of MC68HC908JK3E</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Input-Capture-of-MC68HC908JK3E/m-p/576948#M22113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I use the chip is MC68HC908JK3E, select the timer's channel 1 to capture the external input square wave signal (100-250Hz) period. At the same time, according to the different period, I use timer's channel 0 output adjustable duty cycle square wave signal (20KHz). In the program, I constantly modify the TCH0H and TCH0L to change the duty cycle of the output signal. The current problems are: the capture signal cycle is not accurate, what are the reasons for this? Thank you!&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337726"&gt;code.txt.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Aug 2016 09:05:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Input-Capture-of-MC68HC908JK3E/m-p/576948#M22113</guid>
      <dc:creator>peakgao</dc:creator>
      <dc:date>2016-08-31T09:05:07Z</dc:date>
    </item>
  </channel>
</rss>