<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit Microcontrollers中的主题 Re: Unable to communicate with S08 when FLASH erased</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-communicate-with-S08-when-FLASH-erased/m-p/537265#M22057</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got lost &lt;/P&gt;&lt;P&gt;Would be possible that you explain a little bit?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Jul 2016 21:38:52 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2016-07-07T21:38:52Z</dc:date>
    <item>
      <title>Unable to communicate with S08 when FLASH erased</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-communicate-with-S08-when-FLASH-erased/m-p/537264#M22056</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the debug port of S08 to program it via an external controller. I've noticed that the S08 responds to these pulses via the BKGD PIN only when the FLASH memory is NOT ERASED. I was wondering why this was happening ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jul 2016 09:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-communicate-with-S08-when-FLASH-erased/m-p/537264#M22056</guid>
      <dc:creator>aruraghuwanshi</dc:creator>
      <dc:date>2016-07-05T09:26:08Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to communicate with S08 when FLASH erased</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-communicate-with-S08-when-FLASH-erased/m-p/537265#M22057</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got lost &lt;/P&gt;&lt;P&gt;Would be possible that you explain a little bit?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 21:38:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Unable-to-communicate-with-S08-when-FLASH-erased/m-p/537265#M22057</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-07-07T21:38:52Z</dc:date>
    </item>
  </channel>
</rss>