<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: S08, how to disable pins to decrease power comsuption?</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518745#M22037</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I've read the document.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 15 Jul 2016 01:39:02 GMT</pubDate>
    <dc:creator>w_tension</dc:creator>
    <dc:date>2016-07-15T01:39:02Z</dc:date>
    <item>
      <title>S08, how to disable pins to decrease power comsuption?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518741#M22033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;The DOCs suggest "Configure port pins to minimize current drain", But didn't mention HOW-TO.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 12 Jun 2016 03:27:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518741#M22033</guid>
      <dc:creator>w_tension</dc:creator>
      <dc:date>2016-06-12T03:27:56Z</dc:date>
    </item>
    <item>
      <title>Re: S08, how to disable pins to decrease power comsuption?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518742#M22034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Current drain rises when digital input floats between '0' and '1' levels. To eliminate it do one of the following on all your unused digital inputs:&lt;/P&gt;&lt;P&gt;1) turn input to output using data direction registers&lt;/P&gt;&lt;P&gt;2) enable pull device, both pull-up and pull-down are OK.&lt;/P&gt;&lt;P&gt;3) pull inputs externally to I/O supply rails, usually vss or vdd&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since lower pin count packages may have non bonded out pin pads, you should not forget to turn them into outputs as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edward&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 06:20:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518742#M22034</guid>
      <dc:creator>kef2</dc:creator>
      <dc:date>2016-06-14T06:20:10Z</dc:date>
    </item>
    <item>
      <title>Re: S08, how to disable pins to decrease power comsuption?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518743#M22035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Also remember disable all the modules that you are not using&lt;/P&gt;&lt;P&gt;I do not know the family that you are using but please check the following application note&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4441.pdf?fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1"&gt;AN4441&lt;/A&gt;​&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 16:23:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518743#M22035</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-06-16T16:23:06Z</dc:date>
    </item>
    <item>
      <title>Re: S08, how to disable pins to decrease power comsuption?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518744#M22036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I'm using MC9S08QG4 TSSOP-16.&lt;/P&gt;&lt;P&gt;As I see in its datasheet, Max pin number is 24, So I should take them in count too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 01:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518744#M22036</guid>
      <dc:creator>w_tension</dc:creator>
      <dc:date>2016-07-15T01:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: S08, how to disable pins to decrease power comsuption?</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518745#M22037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, I've read the document.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Jul 2016 01:39:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-how-to-disable-pins-to-decrease-power-comsuption/m-p/518745#M22037</guid>
      <dc:creator>w_tension</dc:creator>
      <dc:date>2016-07-15T01:39:02Z</dc:date>
    </item>
  </channel>
</rss>