<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: S08 SCI LBKD Interrupt</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-LBKD-Interrupt/m-p/508967#M21990</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, can you please tell me the device that you are using&amp;nbsp; (S08) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 May 2016 21:35:38 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2016-05-12T21:35:38Z</dc:date>
    <item>
      <title>S08 SCI LBKD Interrupt</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-LBKD-Interrupt/m-p/508966#M21989</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using S12 communicate with S08 via SCI。When S08 enable the break detect interrupt(set SCIxS2.LBKDE),no ISR reply. See the wave on RX pin with 13clk low, and in debug mode, the SCIxS2.LBKDIF is set. But can not jmp to the ISR.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When S08 disable the break detect inerrupt(clr SCIxS2.LBKDE),the S08 will jmp to ISR with receiver buffer full and Framing Error. I think the baud rate is the same as S12.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 01:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-LBKD-Interrupt/m-p/508966#M21989</guid>
      <dc:creator>qiongyu</dc:creator>
      <dc:date>2016-05-09T01:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: S08 SCI LBKD Interrupt</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-LBKD-Interrupt/m-p/508967#M21990</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, can you please tell me the device that you are using&amp;nbsp; (S08) &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 May 2016 21:35:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/S08-SCI-LBKD-Interrupt/m-p/508967#M21990</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-05-12T21:35:38Z</dc:date>
    </item>
  </channel>
</rss>