<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MC9S08SH4 in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489774#M21863</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i have avr MC9S08SH4 was damage and i have other on good the two avr works on boards i mean pcb. i can bring new MC9S08SH4 and&amp;nbsp; upload the program from the good work one and download the program to the mew on by use Multilink adapter !!!!!?????&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 16 Dec 2015 23:08:42 GMT</pubDate>
    <dc:creator>ameensaleh</dc:creator>
    <dc:date>2015-12-16T23:08:42Z</dc:date>
    <item>
      <title>MC9S08SH4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489774#M21863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i have avr MC9S08SH4 was damage and i have other on good the two avr works on boards i mean pcb. i can bring new MC9S08SH4 and&amp;nbsp; upload the program from the good work one and download the program to the mew on by use Multilink adapter !!!!!?????&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Dec 2015 23:08:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489774#M21863</guid>
      <dc:creator>ameensaleh</dc:creator>
      <dc:date>2015-12-16T23:08:42Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SH4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489775#M21864</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I do not understand your question AVR or freescale?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 01:44:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489775#M21864</guid>
      <dc:creator>Leojunin</dc:creator>
      <dc:date>2015-12-17T01:44:12Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SH4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489776#M21865</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Freescale&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 02:16:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489776#M21865</guid>
      <dc:creator>ameensaleh</dc:creator>
      <dc:date>2015-12-17T02:16:03Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SH4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489777#M21866</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can only access the original firmware if you can pass the following steps:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. The chip operates.&lt;/P&gt;&lt;P&gt;2. The software should not be protected.&lt;/P&gt;&lt;P&gt;3. be protected should be set and meet the backdoor key.&lt;/P&gt;&lt;P&gt;4. If you have not configured the backdoor key you can not read the firmware in any way, unless you can enter it with a routine that give you a serial port and read the firmware and pull out the chip, and go capturing a PC. If well programmed this will not have access to run this routine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have an OS you can access (if you know) the context of a task and change it to run yours, like a virus but is already more complex.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Dec 2015 23:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489777#M21866</guid>
      <dc:creator>Leojunin</dc:creator>
      <dc:date>2015-12-17T23:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SH4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489778#M21867</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you for cooptation....&lt;/P&gt;&lt;P&gt;to do the steps what is the economic interface i can uesd also what is the software i in need ..&lt;/P&gt;&lt;P&gt;thank you again &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Dec 2015 22:11:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489778#M21867</guid>
      <dc:creator>ameensaleh</dc:creator>
      <dc:date>2015-12-21T22:11:40Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S08SH4</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489779#M21868</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI Amenn&lt;/P&gt;&lt;P&gt;I am not sure if you need a OSBDM, if this is the case, you can get the schematics and the firmware, please check the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.pemicro.com/osbdm/" title="http://www.pemicro.com/osbdm/"&gt;P&amp;amp;E Microcomputer Systems&lt;/A&gt; &lt;/P&gt;&lt;P&gt;I hope this will help you&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 17:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/MC9S08SH4/m-p/489779#M21868</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-12-28T17:11:19Z</dc:date>
    </item>
  </channel>
</rss>