<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Mc9s08dz48 background mode error in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476671#M21778</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pedro,&lt;/P&gt;&lt;P&gt;yes, There is no missing part or hardware prob. I just checked. The pcb contains long traces for the crystal. May be thats the reason?&amp;nbsp; &lt;/P&gt;&lt;P&gt;The blue circle is the crystal..and the pins it is routed to. (pin6 and pin7). Mc9s08dz48 is the mcu used for the design.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33761i057E9E8111FB4487/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 11 Jan 2016 21:56:45 GMT</pubDate>
    <dc:creator>saravanananbazh</dc:creator>
    <dc:date>2016-01-11T21:56:45Z</dc:date>
    <item>
      <title>Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476667#M21774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to connect the debugger to the micro thru BKGD pin. i am using PE micro Multilink usb interface. The device connects well and the "target Ready" msg shows up. But when I try to load hex code the programming process stops and shows up with "ERROR 34" message. please find the attached screenshot. ANy help would be appreciated.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Saavy &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="125731_125731.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/120956iDE5003B33F193AEA/image-size/large?v=v2&amp;amp;px=999" role="button" title="125731_125731.png" alt="125731_125731.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55632iA9760E2026C81D8B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jan 2016 19:48:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476667#M21774</guid>
      <dc:creator>saravanananbazh</dc:creator>
      <dc:date>2016-01-08T19:48:37Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476668#M21775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you giving the correct parameters to CPROGHCS08 for your setup?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, I use Cyclone PRO, so it needs: interface=cyclonepro&lt;/P&gt;&lt;P&gt;I also need to specify the port to use: port=xxx.xxx.xxx.xxx (xxx being the Cyclone's IP address)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In your case you need the relevant interface for Multilink (I don't remember what it should be -- multilink? and port usb?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jan 2016 20:04:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476668#M21775</guid>
      <dc:creator>tonyp</dc:creator>
      <dc:date>2016-01-08T20:04:20Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476669#M21776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hell Tony,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the prompt reply. The parameters are correct according to me. This the third project I am working on. The prev two proj were based on same MCU. I never faced such issue before.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jan 2016 20:08:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476669#M21776</guid>
      <dc:creator>saravanananbazh</dc:creator>
      <dc:date>2016-01-08T20:08:20Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476670#M21777</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Saravanan&lt;/P&gt;&lt;P&gt; Are you using your own design, please check that there is not any missing part or hardware problem?&lt;/P&gt;&lt;P&gt;can you check the signal on the reset pin?&lt;/P&gt;&lt;P&gt;if you can share your schematics, please send them&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 21:29:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476670#M21777</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-01-11T21:29:58Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476671#M21778</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pedro,&lt;/P&gt;&lt;P&gt;yes, There is no missing part or hardware prob. I just checked. The pcb contains long traces for the crystal. May be thats the reason?&amp;nbsp; &lt;/P&gt;&lt;P&gt;The blue circle is the crystal..and the pins it is routed to. (pin6 and pin7). Mc9s08dz48 is the mcu used for the design.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33761i057E9E8111FB4487/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Jan 2016 21:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476671#M21778</guid>
      <dc:creator>saravanananbazh</dc:creator>
      <dc:date>2016-01-11T21:56:45Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476672#M21779</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pedro,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I tried using Internal ref clock, But its the same. the software doesnt want to load. I dont know whats wrong. I double checked the hardware and micro pins are properly&amp;nbsp; soldered too.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 21:00:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476672#M21779</guid>
      <dc:creator>saravanananbazh</dc:creator>
      <dc:date>2016-01-13T21:00:04Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476673#M21780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;Have you try to update the multilink? also please send me the schematics of the BKGD connections&lt;/P&gt;&lt;P&gt;have a good day.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 17:56:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476673#M21780</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-01-18T17:56:31Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476674#M21781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;here is the BKGD schematic.. I am using 3 pins (Reset,&amp;nbsp; Gnd and BKGD) instead of 6 pins for BKGD connection.. I did the same for prev projects it worked fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54264i61A366DE7FA4BF70/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 20:57:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476674#M21781</guid>
      <dc:creator>saravanananbazh</dc:creator>
      <dc:date>2016-01-20T20:57:27Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476675#M21782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am getting this error now.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_0.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/54322i069C11E5F5AB6C45/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 21:53:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476675#M21782</guid>
      <dc:creator>saravanananbazh</dc:creator>
      <dc:date>2016-01-20T21:53:57Z</dc:date>
    </item>
    <item>
      <title>Re: Mc9s08dz48 background mode error</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476676#M21783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Please check that the reset pin goes to low, also would be possible that you add a pull up resistor on the reset pin?&lt;/P&gt;&lt;P&gt;I hope this will help you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Jan 2016 15:51:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Mc9s08dz48-background-mode-error/m-p/476676#M21783</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-01-21T15:51:24Z</dc:date>
    </item>
  </channel>
</rss>