<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 3phase BLDC engine program upload in 8-bit Microcontrollers</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469336#M21742</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pawel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have the TWR-MCF51CN?&lt;/P&gt;&lt;P&gt;If this is the case yes, you can program the MC9S08MP16 Controller Daughter Board using the TWR-MCF51CN, you only need to do &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) open the MCU_IDD (J6) on the tower.&lt;/P&gt;&lt;P&gt;2) plug the wire on the J8 also on the tower&lt;/P&gt;&lt;P&gt;3) plug the other side of the wire on the J3 of the daughter MP&lt;/P&gt;&lt;P&gt;4) plug the USB cable on the J14 of the tower&lt;/P&gt;&lt;P&gt;5) Program it using code warrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this help you.&lt;/P&gt;&lt;P&gt;have a good weekend&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Dec 2015 22:08:50 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2015-12-11T22:08:50Z</dc:date>
    <item>
      <title>3phase BLDC engine program upload</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469335#M21741</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have &lt;SPAN style="font-size: 12pt;"&gt;3PHASELV-KIT: 3-Phase BLDC/PMSM Low-Voltage Motor Control Drive and I have a question for that. I'm using it with HCS08MP16 daughter board. I also have MCF51CN board which I want to use as a debugger for my MP16 daughter board.&amp;nbsp; MCF51CN board can be debugged by Mini USB cable. In CodeWarrior 6.3 the connection is viewed as CFV1 FSL Open Source BDM. This is the way I communicate my MCF51CN board with computer. Then I'd like to connect BDM which is on MCF51CN board with BDM on MP16 daughter board. I try to use for it female tape wire like in the picture. I don't have any other BDM programmer and only I can use to upload program on my BLDC engine is BDM on MCF51CN board. &lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="http://lispol.com/uploaded/products_images/1412978901_80059900.jpg"&gt;&lt;IMG alt="http://lispol.com/uploaded/products_images/1412978901_80059900.jpg" class="jive-image" src="http://lispol.com/uploaded/products_images/1412978901_80059900.jpg" /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I don't know how avoid programming of processor on MCF51CN board and send my code on MP16 board to steer the engine. I think it's not impossible.&lt;BR /&gt;If you have any solutions or ideas please help me with it.&lt;BR /&gt;With best regards.&lt;BR /&gt;Pawel Niewiadomski&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Dec 2015 17:09:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469335#M21741</guid>
      <dc:creator>pawelniewiadoms</dc:creator>
      <dc:date>2015-12-08T17:09:58Z</dc:date>
    </item>
    <item>
      <title>Re: 3phase BLDC engine program upload</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469336#M21742</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pawel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have the TWR-MCF51CN?&lt;/P&gt;&lt;P&gt;If this is the case yes, you can program the MC9S08MP16 Controller Daughter Board using the TWR-MCF51CN, you only need to do &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) open the MCU_IDD (J6) on the tower.&lt;/P&gt;&lt;P&gt;2) plug the wire on the J8 also on the tower&lt;/P&gt;&lt;P&gt;3) plug the other side of the wire on the J3 of the daughter MP&lt;/P&gt;&lt;P&gt;4) plug the USB cable on the J14 of the tower&lt;/P&gt;&lt;P&gt;5) Program it using code warrior.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this help you.&lt;/P&gt;&lt;P&gt;have a good weekend&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Dec 2015 22:08:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469336#M21742</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-12-11T22:08:50Z</dc:date>
    </item>
    <item>
      <title>Re: 3phase BLDC engine program upload</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469337#M21743</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I have this board and i did everything you wrote. I even checked BDM signals with oscilloscope and everything seems to be fine. Reset button on both boards (on board TWR-MCF51CN and board of my BLDC) is working in both sides. I can't communicate with it in CodeWarrior 10.6. That;s what happen.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; W&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22162iC5FA9B6E9CC29C93/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When I try to reconnect this shows. &lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/22191i19FF062BD5DB8CB2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Then it's just error when I click 'Abort'. I try to upload empty program with all libraries of MP16 board. Is there any other way to check the communication?&lt;BR /&gt;Greetings,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 12 Dec 2015 00:23:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469337#M21743</guid>
      <dc:creator>pawelniewiadoms</dc:creator>
      <dc:date>2015-12-12T00:23:17Z</dc:date>
    </item>
    <item>
      <title>Re: 3phase BLDC engine program upload</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469338#M21744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pawel&lt;/P&gt;&lt;P&gt;can you check with a Universal multilink (if you have it) if the MP is not damage?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Dec 2015 17:16:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469338#M21744</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-12-28T17:16:25Z</dc:date>
    </item>
    <item>
      <title>Re: 3phase BLDC engine program upload</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469339#M21745</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I removed one of the resistors which send a signal back to th MC on the MCF51CN board and BDM can't support two microprocessors at once. Now TWR board works as programmer very well. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Dec 2015 10:20:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/3phase-BLDC-engine-program-upload/m-p/469339#M21745</guid>
      <dc:creator>pawelniewiadoms</dc:creator>
      <dc:date>2015-12-29T10:20:54Z</dc:date>
    </item>
  </channel>
</rss>