<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックAN3564 USB JM60 question</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN3564-USB-JM60-question/m-p/467005#M21719</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm new in usb world, i want to run&amp;nbsp; AN3564SW1 - Customize your USB application using the JM60_16 projec; i have not JM60 demo board, so i'm building my hardware, but i've some doubt about configuration:&lt;/P&gt;&lt;P&gt;I read on AN that VREG would be configured by USBVREN (USBCTLO) and pull up by USBPU(USBCTLO), so i search in this project for this reference but without success, so i'd like to known if i need to use external or internal 3.3V, external/internal Pullup resistor and if power supply is bus powered or not. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 10 Mar 2016 12:51:01 GMT</pubDate>
    <dc:creator>elettronicarewo</dc:creator>
    <dc:date>2016-03-10T12:51:01Z</dc:date>
    <item>
      <title>AN3564 USB JM60 question</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/AN3564-USB-JM60-question/m-p/467005#M21719</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm new in usb world, i want to run&amp;nbsp; AN3564SW1 - Customize your USB application using the JM60_16 projec; i have not JM60 demo board, so i'm building my hardware, but i've some doubt about configuration:&lt;/P&gt;&lt;P&gt;I read on AN that VREG would be configured by USBVREN (USBCTLO) and pull up by USBPU(USBCTLO), so i search in this project for this reference but without success, so i'd like to known if i need to use external or internal 3.3V, external/internal Pullup resistor and if power supply is bus powered or not. Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Mar 2016 12:51:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/AN3564-USB-JM60-question/m-p/467005#M21719</guid>
      <dc:creator>elettronicarewo</dc:creator>
      <dc:date>2016-03-10T12:51:01Z</dc:date>
    </item>
  </channel>
</rss>