<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: Programming a MC9S08AC128, when I erase a sector with the 0x40 Sector Erase Command upon completion of the erasure FACCERR in the FSTAT register always gets set. This shouldn't be.</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-a-MC9S08AC128-when-I-erase-a-sector-with-the-0x40/m-p/466716#M21717</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;attached is 9s08aw60 flash routine demo code. i suggest you refer it to make yours.&lt;/P&gt;&lt;P&gt;can this help you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Feb 2016 02:29:48 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2016-02-18T02:29:48Z</dc:date>
    <item>
      <title>Programming a MC9S08AC128, when I erase a sector with the 0x40 Sector Erase Command upon completion of the erasure FACCERR in the FSTAT register always gets set. This shouldn't be.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-a-MC9S08AC128-when-I-erase-a-sector-with-the-0x40/m-p/466715#M21716</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Programming a MC9S08AC128, when I erase a sector with the 0x40 Sector Erase Command upon completion of the erasure FACCERR in the FSTAT register always gets set. This shouldn't be.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 00:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-a-MC9S08AC128-when-I-erase-a-sector-with-the-0x40/m-p/466715#M21716</guid>
      <dc:creator>PabloMac</dc:creator>
      <dc:date>2016-02-18T00:40:56Z</dc:date>
    </item>
    <item>
      <title>Re: Programming a MC9S08AC128, when I erase a sector with the 0x40 Sector Erase Command upon completion of the erasure FACCERR in the FSTAT register always gets set. This shouldn't be.</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-a-MC9S08AC128-when-I-erase-a-sector-with-the-0x40/m-p/466716#M21717</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;attached is 9s08aw60 flash routine demo code. i suggest you refer it to make yours.&lt;/P&gt;&lt;P&gt;can this help you?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jennie Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Feb 2016 02:29:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Programming-a-MC9S08AC128-when-I-erase-a-sector-with-the-0x40/m-p/466716#M21717</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2016-02-18T02:29:48Z</dc:date>
    </item>
  </channel>
</rss>