<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックFunction works without declaration</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Function-works-without-declaration/m-p/466355#M21710</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I am using &lt;EM&gt;&lt;STRONG&gt;MC9s08pa16&lt;/STRONG&gt;&lt;/EM&gt; for my bldc motor project with &lt;EM&gt;&lt;STRONG&gt;code warrior v 10.6&lt;/STRONG&gt;&lt;/EM&gt;. I have rpm control function in my project. &lt;EM&gt;&lt;STRONG&gt;do_rpm_calc &lt;/STRONG&gt;&lt;/EM&gt;is&amp;nbsp; my function. I have defined the function as &lt;EM&gt;&lt;STRONG&gt;do_rpm_calc&lt;/STRONG&gt;&lt;/EM&gt;&lt;STRONG&gt; &lt;/STRONG&gt; but i ve declared it as&lt;EM&gt;&lt;STRONG&gt; do_calc_rpm.&lt;/STRONG&gt;&lt;/EM&gt;&lt;STRONG&gt; &lt;/STRONG&gt; My code works fine and compiler doesnt throw the error. I have created .SAP file and gave it to the production. Will there be any problem in the future?. Why the compiler doesnt throw the error?. How come the code works fine?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;A.Kathirkamu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 21 Apr 2016 09:43:24 GMT</pubDate>
    <dc:creator>kathirkamuannak</dc:creator>
    <dc:date>2016-04-21T09:43:24Z</dc:date>
    <item>
      <title>Function works without declaration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Function-works-without-declaration/m-p/466355#M21710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;I am using &lt;EM&gt;&lt;STRONG&gt;MC9s08pa16&lt;/STRONG&gt;&lt;/EM&gt; for my bldc motor project with &lt;EM&gt;&lt;STRONG&gt;code warrior v 10.6&lt;/STRONG&gt;&lt;/EM&gt;. I have rpm control function in my project. &lt;EM&gt;&lt;STRONG&gt;do_rpm_calc &lt;/STRONG&gt;&lt;/EM&gt;is&amp;nbsp; my function. I have defined the function as &lt;EM&gt;&lt;STRONG&gt;do_rpm_calc&lt;/STRONG&gt;&lt;/EM&gt;&lt;STRONG&gt; &lt;/STRONG&gt; but i ve declared it as&lt;EM&gt;&lt;STRONG&gt; do_calc_rpm.&lt;/STRONG&gt;&lt;/EM&gt;&lt;STRONG&gt; &lt;/STRONG&gt; My code works fine and compiler doesnt throw the error. I have created .SAP file and gave it to the production. Will there be any problem in the future?. Why the compiler doesnt throw the error?. How come the code works fine?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;A.Kathirkamu&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Apr 2016 09:43:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Function-works-without-declaration/m-p/466355#M21710</guid>
      <dc:creator>kathirkamuannak</dc:creator>
      <dc:date>2016-04-21T09:43:24Z</dc:date>
    </item>
    <item>
      <title>Re: Function works without declaration</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/Function-works-without-declaration/m-p/466356#M21711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;I believe that the code is not working properly &lt;/P&gt;&lt;P&gt;Would be possible that you send me your project, if you can not share on the community your code, you can create a case request on the nxp web page and send the project on it and it will be private.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Apr 2016 00:41:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/Function-works-without-declaration/m-p/466356#M21711</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2016-04-27T00:41:21Z</dc:date>
    </item>
  </channel>
</rss>