<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>8-bit MicrocontrollersのトピックRe: TWR=MCF51CN Bootloader Mode problem</title>
    <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TWR-MCF51CN-Bootloader-Mode-problem/m-p/461414#M21697</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pawel&lt;/P&gt;&lt;P&gt;The J16 is only use if you want to update the firmware on the JM60 (OSBDM), if this is present you only can update the firmware with the P&amp;amp;E tools.&lt;/P&gt;&lt;P&gt;If you want to program the MCF51CN you need to remove the J16.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Dec 2015 22:22:59 GMT</pubDate>
    <dc:creator>vicentegomez</dc:creator>
    <dc:date>2015-12-11T22:22:59Z</dc:date>
    <item>
      <title>TWR=MCF51CN Bootloader Mode problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TWR-MCF51CN-Bootloader-Mode-problem/m-p/461413#M21696</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have TWR-MCF51CN board and I have problem with bootloader mode in it. When I want to update my firmware by P&amp;amp;E firmware updater I have to use jumper on J16. When I've done it my device become undetected. When I use CodeWarrior v10.6.4 it also makes update of my firmware and it's the same problem. It happens when I reconnect my board with jumper on. Without jumper on J16 my device is detected. I'm using Mini USB cable as debugger.&lt;/P&gt;&lt;P&gt;Thanks for all responses.&lt;/P&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;Pawel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Dec 2015 23:24:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TWR-MCF51CN-Bootloader-Mode-problem/m-p/461413#M21696</guid>
      <dc:creator>pawelniewiadoms</dc:creator>
      <dc:date>2015-12-03T23:24:53Z</dc:date>
    </item>
    <item>
      <title>Re: TWR=MCF51CN Bootloader Mode problem</title>
      <link>https://community.nxp.com/t5/8-bit-Microcontrollers/TWR-MCF51CN-Bootloader-Mode-problem/m-p/461414#M21697</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pawel&lt;/P&gt;&lt;P&gt;The J16 is only use if you want to update the firmware on the JM60 (OSBDM), if this is present you only can update the firmware with the P&amp;amp;E tools.&lt;/P&gt;&lt;P&gt;If you want to program the MCF51CN you need to remove the J16.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Vicente Gomez&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Dec 2015 22:22:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/8-bit-Microcontrollers/TWR-MCF51CN-Bootloader-Mode-problem/m-p/461414#M21697</guid>
      <dc:creator>vicentegomez</dc:creator>
      <dc:date>2015-12-11T22:22:59Z</dc:date>
    </item>
  </channel>
</rss>